<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Multiple HW configurations in one project in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Multiple-HW-configurations-in-one-project/m-p/1773771#M29575</link>
    <description>&lt;P&gt;Hi Everyone!&lt;/P&gt;&lt;P&gt;We have a software project which we use on multiple revisions of HW, where the used package of the MCU (s32k358) and also the pinout is different. We would like to have multiple *.mex files in the same project for the different HW configs. As far as I understand, this is not possible due to the limitations in how S32DS handles these configuration files. Is there any kind of non-hacky way to do something like this?&lt;/P&gt;</description>
    <pubDate>Wed, 13 Dec 2023 09:19:10 GMT</pubDate>
    <dc:creator>ferenczyg</dc:creator>
    <dc:date>2023-12-13T09:19:10Z</dc:date>
    <item>
      <title>Multiple HW configurations in one project</title>
      <link>https://community.nxp.com/t5/S32K/Multiple-HW-configurations-in-one-project/m-p/1773771#M29575</link>
      <description>&lt;P&gt;Hi Everyone!&lt;/P&gt;&lt;P&gt;We have a software project which we use on multiple revisions of HW, where the used package of the MCU (s32k358) and also the pinout is different. We would like to have multiple *.mex files in the same project for the different HW configs. As far as I understand, this is not possible due to the limitations in how S32DS handles these configuration files. Is there any kind of non-hacky way to do something like this?&lt;/P&gt;</description>
      <pubDate>Wed, 13 Dec 2023 09:19:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Multiple-HW-configurations-in-one-project/m-p/1773771#M29575</guid>
      <dc:creator>ferenczyg</dc:creator>
      <dc:date>2023-12-13T09:19:10Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple HW configurations in one project</title>
      <link>https://community.nxp.com/t5/S32K/Multiple-HW-configurations-in-one-project/m-p/1774181#M29591</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/226988"&gt;@ferenczyg&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Check the following community post. It has information related to a property of ConfigTools that might be useful for you.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio/How-to-create-different-hardware-configuration-for-different/m-p/1373580" target="_blank" rel="noopener"&gt;How to create different hardware configurations for different builds within one project.&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R.&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;</description>
      <pubDate>Wed, 13 Dec 2023 21:08:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Multiple-HW-configurations-in-one-project/m-p/1774181#M29591</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-12-13T21:08:26Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple HW configurations in one project</title>
      <link>https://community.nxp.com/t5/S32K/Multiple-HW-configurations-in-one-project/m-p/1774872#M29631</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;VaneB,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks for the reply. Unfortunately, this does not solve my issue. I need to be able to change the package (MQFP172 vs BGA289) as well, not just the pin configs.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Dec 2023 14:32:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Multiple-HW-configurations-in-one-project/m-p/1774872#M29631</guid>
      <dc:creator>ferenczyg</dc:creator>
      <dc:date>2023-12-14T14:32:27Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple HW configurations in one project</title>
      <link>https://community.nxp.com/t5/S32K/Multiple-HW-configurations-in-one-project/m-p/1775154#M29638</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/226988"&gt;@ferenczyg&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Sorry for the misunderstanding.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I am going to use the LpuartFlexio_Uart_Ip_Example_S32K344 code as a reference. When you create this project from example, no changes need to be done to run it in the S32K344-T172EVB and S32K344-Q257EVB, and if you see the project by default use 257package. If you change the package to 172 the following changes are done:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="VaneB_0-1702594557638.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/254562i7BDFE85AD829A00F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="VaneB_0-1702594557638.png" alt="VaneB_0-1702594557638.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="VaneB_1-1702594571356.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/254563iFD3E836FFE9E622C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="VaneB_1-1702594571356.png" alt="VaneB_1-1702594571356.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;As you can see, the only changes made are some comments, but the pin's configuration does not change. This means that if you create the project for one package should work for the other one. &lt;BR /&gt;Just take into consideration the difference in the number of pins.&lt;/P&gt;</description>
      <pubDate>Thu, 14 Dec 2023 23:03:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Multiple-HW-configurations-in-one-project/m-p/1775154#M29638</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-12-14T23:03:12Z</dc:date>
    </item>
  </channel>
</rss>