<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MCU_HSE_SWT_RST_RESET in S32K</title>
    <link>https://community.nxp.com/t5/S32K/MCU-HSE-SWT-RST-RESET/m-p/1769208#M29332</link>
    <description>&lt;P&gt;S32K388 Eval Board resets with reason&amp;nbsp;MCU_HSE_SWT_RST_RESET&lt;BR /&gt;- The Eval board resets only one time after the startup and then work normally&lt;BR /&gt;- Why this happens?&lt;BR /&gt;- I tried to write directly to&amp;nbsp;DCMRWP1 register to disable the functional reset but nothing happened.&lt;BR /&gt;Update:&lt;BR /&gt;Also,&amp;nbsp;Siul2_Port_Ip_Example_S32K388 which is supported from s32k388 package does the same behavior.&lt;BR /&gt;- The Software should toggle the LED on PTA0 10 times&lt;BR /&gt;- After powering up the LED starts with 3 blinks the resets and begin to blink 10 times&lt;/P&gt;</description>
    <pubDate>Wed, 06 Dec 2023 15:35:04 GMT</pubDate>
    <dc:creator>myehiash</dc:creator>
    <dc:date>2023-12-06T15:35:04Z</dc:date>
    <item>
      <title>MCU_HSE_SWT_RST_RESET</title>
      <link>https://community.nxp.com/t5/S32K/MCU-HSE-SWT-RST-RESET/m-p/1769208#M29332</link>
      <description>&lt;P&gt;S32K388 Eval Board resets with reason&amp;nbsp;MCU_HSE_SWT_RST_RESET&lt;BR /&gt;- The Eval board resets only one time after the startup and then work normally&lt;BR /&gt;- Why this happens?&lt;BR /&gt;- I tried to write directly to&amp;nbsp;DCMRWP1 register to disable the functional reset but nothing happened.&lt;BR /&gt;Update:&lt;BR /&gt;Also,&amp;nbsp;Siul2_Port_Ip_Example_S32K388 which is supported from s32k388 package does the same behavior.&lt;BR /&gt;- The Software should toggle the LED on PTA0 10 times&lt;BR /&gt;- After powering up the LED starts with 3 blinks the resets and begin to blink 10 times&lt;/P&gt;</description>
      <pubDate>Wed, 06 Dec 2023 15:35:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MCU-HSE-SWT-RST-RESET/m-p/1769208#M29332</guid>
      <dc:creator>myehiash</dc:creator>
      <dc:date>2023-12-06T15:35:04Z</dc:date>
    </item>
  </channel>
</rss>