<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K debug password usage without HSE in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K-debug-password-usage-without-HSE/m-p/1768234#M29286</link>
    <description>Thanks for the reply.&lt;BR /&gt;Once Password is set and LC is moved to In-FIELD,&lt;BR /&gt;1. Is it possible to flash Binaries over JTAG again by providing password? If yes, then how?&lt;BR /&gt;2. Debug can be done in same LC state or it needs to be moved to other state?</description>
    <pubDate>Mon, 04 Dec 2023 11:27:38 GMT</pubDate>
    <dc:creator>BhushanM</dc:creator>
    <dc:date>2023-12-04T11:27:38Z</dc:date>
    <item>
      <title>S32K debug password usage without HSE</title>
      <link>https://community.nxp.com/t5/S32K/S32K-debug-password-usage-without-HSE/m-p/1767210#M29236</link>
      <description>&lt;P&gt;Hello Team,&lt;/P&gt;&lt;P&gt;Is it possible to secure the JTAG usage by setting password inside "CUST_DB_PSWD_A" register without installing or enabling HSE FW?&lt;/P&gt;&lt;P&gt;If yes, then could you also provide steps how to take secure access for same by providing password over SEGGER.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Bhushan Mahale&lt;/P&gt;</description>
      <pubDate>Fri, 01 Dec 2023 10:21:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-debug-password-usage-without-HSE/m-p/1767210#M29236</guid>
      <dc:creator>BhushanM</dc:creator>
      <dc:date>2023-12-01T10:21:25Z</dc:date>
    </item>
    <item>
      <title>Re: S32K debug password usage without HSE</title>
      <link>https://community.nxp.com/t5/S32K/S32K-debug-password-usage-without-HSE/m-p/1767864#M29263</link>
      <description>&lt;P&gt;Please do reply.&lt;/P&gt;</description>
      <pubDate>Mon, 04 Dec 2023 03:51:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-debug-password-usage-without-HSE/m-p/1767864#M29263</guid>
      <dc:creator>BhushanM</dc:creator>
      <dc:date>2023-12-04T03:51:27Z</dc:date>
    </item>
    <item>
      <title>Re: S32K debug password usage without HSE</title>
      <link>https://community.nxp.com/t5/S32K/S32K-debug-password-usage-without-HSE/m-p/1768223#M29284</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;Is it possible to secure the JTAG usage by setting password inside "CUST_DB_PSWD_A" register without installing or enabling HSE FW?&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Yes, it is.&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;If yes, then could you also provide steps how to take secure access for same by providing password over SEGGER.&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;We do not use segger here, but you can follow the general steps for any programmer.&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;1.&lt;/STRONG&gt; Set up ADKP (Application Debug Key/Password).&lt;BR /&gt;&lt;STRONG&gt;2.&lt;/STRONG&gt; Make sure the password mode or challenge-response mode.&lt;BR /&gt;&lt;STRONG&gt;3.&lt;/STRONG&gt; Move the lifecycle to the IN-FIELD stage.&lt;/P&gt;
&lt;P&gt;Please see the following thread where it is explained in details:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Restrict-the-debug-access-with-a-password-when-HSE-is-not/ta-p/1735073" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Restrict-the-debug-access-with-a-password-when-HSE-is-not/ta-p/1735073&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Mon, 04 Dec 2023 11:05:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-debug-password-usage-without-HSE/m-p/1768223#M29284</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2023-12-04T11:05:45Z</dc:date>
    </item>
    <item>
      <title>Re: S32K debug password usage without HSE</title>
      <link>https://community.nxp.com/t5/S32K/S32K-debug-password-usage-without-HSE/m-p/1768234#M29286</link>
      <description>Thanks for the reply.&lt;BR /&gt;Once Password is set and LC is moved to In-FIELD,&lt;BR /&gt;1. Is it possible to flash Binaries over JTAG again by providing password? If yes, then how?&lt;BR /&gt;2. Debug can be done in same LC state or it needs to be moved to other state?</description>
      <pubDate>Mon, 04 Dec 2023 11:27:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-debug-password-usage-without-HSE/m-p/1768234#M29286</guid>
      <dc:creator>BhushanM</dc:creator>
      <dc:date>2023-12-04T11:27:38Z</dc:date>
    </item>
    <item>
      <title>Re: S32K debug password usage without HSE</title>
      <link>https://community.nxp.com/t5/S32K/S32K-debug-password-usage-without-HSE/m-p/1769641#M29359</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;1. Is it possible to flash Binaries over JTAG again by providing password? If yes, then how?&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Yes. This is question for your debugger vendor.&lt;/P&gt;
&lt;P&gt;For example PE Micro:&lt;/P&gt;
&lt;P&gt;To unlock the MCU, PEmicro provides some Python scripts (PEmicro support files package) to facilitate the authentication of the debugger when the password is set.&lt;/P&gt;
&lt;P&gt;Once the debug session is established, you will do simple programming to device as normal.&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;2. Debug can be done in same LC state or it needs to be moved to other state?&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Debug can be done in any lice cycle. You advance life cycle to mature security.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 06 Dec 2023 09:05:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-debug-password-usage-without-HSE/m-p/1769641#M29359</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2023-12-06T09:05:29Z</dc:date>
    </item>
  </channel>
</rss>