<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SWD problem on s32k144 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/SWD-problem-on-s32k144/m-p/810202#M2927</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV class=""&gt;&lt;P&gt;I have successfully programmed my device but now I cannot connect with MCU.&lt;/P&gt;&lt;P&gt;I use SWD interface. It can be the case that I use SWD pins as output and in my code I set PTA4 and PTA5 as output. Can it be the case?&lt;/P&gt;What can I do? &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Aug 2018 19:05:00 GMT</pubDate>
    <dc:creator>lohrsistemas</dc:creator>
    <dc:date>2018-08-21T19:05:00Z</dc:date>
    <item>
      <title>SWD problem on s32k144</title>
      <link>https://community.nxp.com/t5/S32K/SWD-problem-on-s32k144/m-p/810202#M2927</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV class=""&gt;&lt;P&gt;I have successfully programmed my device but now I cannot connect with MCU.&lt;/P&gt;&lt;P&gt;I use SWD interface. It can be the case that I use SWD pins as output and in my code I set PTA4 and PTA5 as output. Can it be the case?&lt;/P&gt;What can I do? &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Aug 2018 19:05:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SWD-problem-on-s32k144/m-p/810202#M2927</guid>
      <dc:creator>lohrsistemas</dc:creator>
      <dc:date>2018-08-21T19:05:00Z</dc:date>
    </item>
    <item>
      <title>Re: SWD problem on s32k144</title>
      <link>https://community.nxp.com/t5/S32K/SWD-problem-on-s32k144/m-p/810203#M2928</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;It seems to be the case.&lt;/P&gt;&lt;P&gt;It was discussed in this thread:&amp;nbsp;&lt;A href="https://community.nxp.com/message/987643"&gt;https://community.nxp.com/message/987643&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can use the PEmicro recovery utility mentioned in the thread.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Aug 2018 21:06:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SWD-problem-on-s32k144/m-p/810203#M2928</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-08-21T21:06:41Z</dc:date>
    </item>
    <item>
      <title>Re: SWD problem on s32k144</title>
      <link>https://community.nxp.com/t5/S32K/SWD-problem-on-s32k144/m-p/810204#M2929</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN&gt;Hi Daniel,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I did not have the hardware PE micro, so I tried with the SEGGER.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Trying several times to reset the power of my board, had a moment when I was able to program it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;Okay, that saved my board.&lt;/SPAN&gt; &lt;SPAN class=""&gt;However I will go through this problem if I have to use these pins in a project where the pins of the MCU are completely used, and the last resort is to share the SWD pins.&lt;/SPAN&gt; &lt;SPAN class=""&gt;I suggest having some commentary on the datasheet of this item, guiding the risks of using SWD pins for general purposes.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Aug 2018 11:28:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SWD-problem-on-s32k144/m-p/810204#M2929</guid>
      <dc:creator>lohrsistemas</dc:creator>
      <dc:date>2018-08-22T11:28:26Z</dc:date>
    </item>
  </channel>
</rss>