<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K312 : Communication error with the peripheral when using LPSPI with DMA in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K312-Communication-error-with-the-peripheral-when-using-LPSPI/m-p/1766509#M29195</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;usually issues is due to cache enabled, so put buffers into non-cacheable area.&lt;BR /&gt;If does not help, share full simplified project so can be tested.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Thu, 30 Nov 2023 12:41:09 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2023-11-30T12:41:09Z</dc:date>
    <item>
      <title>S32K312 : Communication error with the peripheral when using LPSPI with DMA</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-Communication-error-with-the-peripheral-when-using-LPSPI/m-p/1765688#M29150</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;I am facing problem when using LPSPI with DMA to communicate with the peripheral on S32K312 controller, as you can see from the DSO output attached below, when initiating the transmission the MOSI pin stays low even though we are sending the data. When tried with normal LPSPI without DMA, it works correctly.&lt;/P&gt;&lt;P&gt;After the transmission is completed neither the SPI nor DMA has any error flags set. I am attaching the&amp;nbsp; of TCD configuration of RX and TX channel just before&amp;nbsp;&lt;SPAN&gt;&lt;SPAN class=""&gt;DMA request is enabled on SPI side.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;What could be causing this issue ?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;Note : &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;CH0 is used for RX and CH1 is used for TX&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;eDMA CSR register has&amp;nbsp;GMRC, ERCA, EDBG, HAE&amp;nbsp; bits enabled&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;</description>
      <pubDate>Wed, 29 Nov 2023 12:32:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-Communication-error-with-the-peripheral-when-using-LPSPI/m-p/1765688#M29150</guid>
      <dc:creator>amangandhi98</dc:creator>
      <dc:date>2023-11-29T12:32:21Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 : Communication error with the peripheral when using LPSPI with DMA</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-Communication-error-with-the-peripheral-when-using-LPSPI/m-p/1766509#M29195</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;usually issues is due to cache enabled, so put buffers into non-cacheable area.&lt;BR /&gt;If does not help, share full simplified project so can be tested.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Thu, 30 Nov 2023 12:41:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-Communication-error-with-the-peripheral-when-using-LPSPI/m-p/1766509#M29195</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-11-30T12:41:09Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 : Communication error with the peripheral when using LPSPI with DMA</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-Communication-error-with-the-peripheral-when-using-LPSPI/m-p/1767899#M29266</link>
      <description>Thanks for the help, assigning the buffers to non-cacheable area worked.</description>
      <pubDate>Mon, 04 Dec 2023 05:46:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-Communication-error-with-the-peripheral-when-using-LPSPI/m-p/1767899#M29266</guid>
      <dc:creator>amangandhi98</dc:creator>
      <dc:date>2023-12-04T05:46:43Z</dc:date>
    </item>
  </channel>
</rss>