<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: PIT TRGMUX</title>
    <link>https://community.nxp.com/t5/S32K/PIT-TRGMUX/m-p/1765435#M29128</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;I have configured TRGMUX on S32K1 to select the same &lt;STRONG&gt;Hardware Input&lt;/STRONG&gt; for two different &lt;STRONG&gt;Hardware Output&lt;/STRONG&gt;. So I think this is also feasible on S32K3.&lt;BR /&gt;You can test if it works.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;/P&gt;</description>
    <pubDate>Wed, 29 Nov 2023 06:41:00 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2023-11-29T06:41:00Z</dc:date>
    <item>
      <title>PIT TRGMUX</title>
      <link>https://community.nxp.com/t5/S32K/PIT-TRGMUX/m-p/1764637#M29060</link>
      <description>&lt;P&gt;I have 8 channels configured on ADC0 and 3 channels configured on ADC1. Can I use one PIT channel(PIT0 CH0) to trigger 2 TRGMUX hardware input which in turn trigger ADC0 and ADC1 respectively. Will this start parallel conv of ADC0 and 1.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="enthuCutlet_0-1701156644195.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/251793i415F6EFE6C50BC9E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="enthuCutlet_0-1701156644195.png" alt="enthuCutlet_0-1701156644195.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;enthuCutlet_0-1701156644195.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="enthuCutlet_1-1701156690150.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/251794iBC8CC643123BB230/image-size/medium?v=v2&amp;amp;px=400" role="button" title="enthuCutlet_1-1701156690150.png" alt="enthuCutlet_1-1701156690150.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;enthuCutlet_1-1701156690150.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 28 Nov 2023 07:32:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/PIT-TRGMUX/m-p/1764637#M29060</guid>
      <dc:creator>enthuCutlet</dc:creator>
      <dc:date>2023-11-28T07:32:00Z</dc:date>
    </item>
    <item>
      <title>Re: PIT TRGMUX</title>
      <link>https://community.nxp.com/t5/S32K/PIT-TRGMUX/m-p/1765435#M29128</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;I have configured TRGMUX on S32K1 to select the same &lt;STRONG&gt;Hardware Input&lt;/STRONG&gt; for two different &lt;STRONG&gt;Hardware Output&lt;/STRONG&gt;. So I think this is also feasible on S32K3.&lt;BR /&gt;You can test if it works.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;/P&gt;</description>
      <pubDate>Wed, 29 Nov 2023 06:41:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/PIT-TRGMUX/m-p/1765435#M29128</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-11-29T06:41:00Z</dc:date>
    </item>
  </channel>
</rss>