<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic urgent help needed: the project uplevel folder is gone while renaming the project in S32DS in S32K</title>
    <link>https://community.nxp.com/t5/S32K/urgent-help-needed-the-project-uplevel-folder-is-gone-while/m-p/1765036#M29100</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Using S32DS version 3.5, when I rename a project, the project is gone in S32DS, also not available in the hard disk any more. Not only that, the whole uplevel folder is gone with all the projects in that folder.&lt;/P&gt;&lt;P&gt;The operation is right clicking the project, then clicking "rename", a window pops up with the uplevel folder name. With a little hesitation, I still changed the name, then the whole uplevel folder is gone. Can this folder be found back, or it is completely deleted from the hard disk?&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is the right operation to change a project's name?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Crane&lt;/P&gt;</description>
    <pubDate>Tue, 28 Nov 2023 16:06:28 GMT</pubDate>
    <dc:creator>cranes</dc:creator>
    <dc:date>2023-11-28T16:06:28Z</dc:date>
    <item>
      <title>urgent help needed: the project uplevel folder is gone while renaming the project in S32DS</title>
      <link>https://community.nxp.com/t5/S32K/urgent-help-needed-the-project-uplevel-folder-is-gone-while/m-p/1765036#M29100</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Using S32DS version 3.5, when I rename a project, the project is gone in S32DS, also not available in the hard disk any more. Not only that, the whole uplevel folder is gone with all the projects in that folder.&lt;/P&gt;&lt;P&gt;The operation is right clicking the project, then clicking "rename", a window pops up with the uplevel folder name. With a little hesitation, I still changed the name, then the whole uplevel folder is gone. Can this folder be found back, or it is completely deleted from the hard disk?&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is the right operation to change a project's name?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Crane&lt;/P&gt;</description>
      <pubDate>Tue, 28 Nov 2023 16:06:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/urgent-help-needed-the-project-uplevel-folder-is-gone-while/m-p/1765036#M29100</guid>
      <dc:creator>cranes</dc:creator>
      <dc:date>2023-11-28T16:06:28Z</dc:date>
    </item>
    <item>
      <title>Re: urgent help needed: the project uplevel folder is gone while renaming the project in S32DS</title>
      <link>https://community.nxp.com/t5/S32K/urgent-help-needed-the-project-uplevel-folder-is-gone-while/m-p/1765198#M29106</link>
      <description>&lt;P&gt;It looks that it works fine to rename the project if the project is in the workspace folder.&amp;nbsp;&lt;/P&gt;&lt;P&gt;It happens when the project is in a subfolder in the workspace folder.&lt;/P&gt;</description>
      <pubDate>Tue, 28 Nov 2023 22:20:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/urgent-help-needed-the-project-uplevel-folder-is-gone-while/m-p/1765198#M29106</guid>
      <dc:creator>cranes</dc:creator>
      <dc:date>2023-11-28T22:20:11Z</dc:date>
    </item>
    <item>
      <title>Re: urgent help needed: the project uplevel folder is gone while renaming the project in S32DS</title>
      <link>https://community.nxp.com/t5/S32K/urgent-help-needed-the-project-uplevel-folder-is-gone-while/m-p/1767192#M29232</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I have tried it on my end and it is working properly.&lt;/P&gt;
&lt;P&gt;The folder should be officially there so it will propagate to .xml file&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Fri, 01 Dec 2023 09:51:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/urgent-help-needed-the-project-uplevel-folder-is-gone-while/m-p/1767192#M29232</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2023-12-01T09:51:32Z</dc:date>
    </item>
  </channel>
</rss>