<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32k324 SysTick</title>
    <link>https://community.nxp.com/t5/S32K/S32k324-SysTick/m-p/1764761#M29076</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Systick belongs to ARM Cortex-M7 Core. S32K324 has two Cortex-M7 Cores. But the Systick is an optional feature so I'm not sure if it's implemented on every M7 core. (&lt;A href="https://developer.arm.com/documentation/101407/0538/Debugging/Debug-Windows-and-Dialogs/Core-Peripherals/Armv7-M-cores/Armv7-M--System-Tick-Timer" target="_self"&gt;Armv7-M: System Tick Timer&lt;/A&gt;)&lt;BR /&gt;Sorry, I don't have S32K324 around to test. If it is convenient, you can try to access the Systick of the two cores separately during debugging to see if they exist.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;/P&gt;</description>
    <pubDate>Tue, 28 Nov 2023 09:15:21 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2023-11-28T09:15:21Z</dc:date>
    <item>
      <title>S32k324 SysTick</title>
      <link>https://community.nxp.com/t5/S32K/S32k324-SysTick/m-p/1764082#M29040</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are currently developing on MCU s32k324.&lt;BR /&gt;I wanted to know if the SysTick peripheral was unique per Core or was only one instance of it in the MCU?&lt;BR /&gt;I mean, does each core have a SysTick peripheral or is there only one SysTick in general.&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;</description>
      <pubDate>Mon, 27 Nov 2023 14:17:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k324-SysTick/m-p/1764082#M29040</guid>
      <dc:creator>Simone9</dc:creator>
      <dc:date>2023-11-27T14:17:59Z</dc:date>
    </item>
    <item>
      <title>Re: S32k324 SysTick</title>
      <link>https://community.nxp.com/t5/S32K/S32k324-SysTick/m-p/1764761#M29076</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Systick belongs to ARM Cortex-M7 Core. S32K324 has two Cortex-M7 Cores. But the Systick is an optional feature so I'm not sure if it's implemented on every M7 core. (&lt;A href="https://developer.arm.com/documentation/101407/0538/Debugging/Debug-Windows-and-Dialogs/Core-Peripherals/Armv7-M-cores/Armv7-M--System-Tick-Timer" target="_self"&gt;Armv7-M: System Tick Timer&lt;/A&gt;)&lt;BR /&gt;Sorry, I don't have S32K324 around to test. If it is convenient, you can try to access the Systick of the two cores separately during debugging to see if they exist.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;/P&gt;</description>
      <pubDate>Tue, 28 Nov 2023 09:15:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k324-SysTick/m-p/1764761#M29076</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-11-28T09:15:21Z</dc:date>
    </item>
  </channel>
</rss>