<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32k310 wake up</title>
    <link>https://community.nxp.com/t5/S32K/S32k310-wake-up/m-p/1763464#M28980</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/138997"&gt;@hajianik&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I think that this could help:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Low-Power-Management-AN-and-demos/ta-p/1527724" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Low-Power-Management-AN-and-demos/ta-p/1527724&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;There's also example for wake-up via GPIO.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
    <pubDate>Fri, 24 Nov 2023 17:27:33 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2023-11-24T17:27:33Z</dc:date>
    <item>
      <title>S32k310 wake up</title>
      <link>https://community.nxp.com/t5/S32K/S32k310-wake-up/m-p/1762247#M28898</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using the S32K310 EVAL BOARD Q100.&lt;/P&gt;&lt;P&gt;I'm able to set the device to standby mode but I can't wake it up, I have configured the pin PTC11 as WKPU_18&amp;nbsp; in pin configuration module . This is a switch input on the q100 board.&lt;/P&gt;&lt;P&gt;I've also configured the wakeup module to for the interrupt and give the &lt;STRONG&gt;HARDWARE CHANNEL&lt;/STRONG&gt; &lt;STRONG&gt;NUMBER AS 22&lt;/STRONG&gt;(AN OFFSET OF 4)since the 1st 4 channels are used for internal wake up.&lt;/P&gt;&lt;P&gt;This is the code snippet I'm testing. I know I have not switch to IFRC. may be that is the issue.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;IntCtrl_Ip_EnableIrq(83);&lt;BR /&gt;Wkpu_Ip_Init (0, &amp;amp;Wkpu_Ip_Config_PB);&lt;BR /&gt;Wkpu_Ip_EnableInterrupt(0, Wkpu_Ip_ChannelConfig_PB[0].hwChannel);&lt;BR /&gt;&lt;BR /&gt;Power_Ip_SetMode(&amp;amp;Power_Ip_aModeConfigPB[0]);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is not working for me . All the generated structures are as expected and I SEE THE PROPER REGISTER IN THE WAKEUP module are populated&amp;nbsp; correctly.&lt;/P&gt;&lt;P&gt;The clk for wakeup module are enabled and active. Also in POWER CONFIGURATION&amp;nbsp; for standby ,clocks through partitions 0/1 are enabled. I don't know what is going on.&lt;/P&gt;&lt;P&gt;Please educate me.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Koorosh Hajiani&lt;/P&gt;</description>
      <pubDate>Thu, 23 Nov 2023 00:51:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k310-wake-up/m-p/1762247#M28898</guid>
      <dc:creator>hajianik</dc:creator>
      <dc:date>2023-11-23T00:51:49Z</dc:date>
    </item>
    <item>
      <title>Re: S32k310 wake up</title>
      <link>https://community.nxp.com/t5/S32K/S32k310-wake-up/m-p/1763464#M28980</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/138997"&gt;@hajianik&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I think that this could help:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Low-Power-Management-AN-and-demos/ta-p/1527724" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Low-Power-Management-AN-and-demos/ta-p/1527724&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;There's also example for wake-up via GPIO.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Fri, 24 Nov 2023 17:27:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k310-wake-up/m-p/1763464#M28980</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2023-11-24T17:27:33Z</dc:date>
    </item>
    <item>
      <title>Re: S32k310 wake up</title>
      <link>https://community.nxp.com/t5/S32K/S32k310-wake-up/m-p/1763502#M28983</link>
      <description>&lt;P&gt;Hi&amp;nbsp; &amp;nbsp;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/37795" target="_self"&gt;&lt;SPAN class=""&gt;Luka,&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Thank you for your response.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I looked at the example in the link you send. They are not targeted for S32k310 eval board that I have so I can't run them but I can compile them.&amp;nbsp; I looked at example "S32K344_GPIO_Wkup_S32DS_3_4_RTD_LLD_2_0" the configuration for POWER and WAKUP are identical to mine except for the wakeup pin that is specific to the board I'm using.&lt;/P&gt;&lt;P&gt;THE ONLY DIFFERENCE IS THEY SWITH THE CLOCK TO IFRC , BEFORE THEY ENTER STANDBY MODE.&lt;/P&gt;&lt;P&gt;I'm lost, When I run my code all the relevant registers appear to show the value that I expected. I don't know if 32K310 honor the wakeup interrupt or not , as I said it goes to to standby mode and the only way to wake it up is via a reset.&lt;/P&gt;&lt;P&gt;what else could be the issue? I need all the help I can get&amp;nbsp; for this issue.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Koorosh Hajiani&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 25 Nov 2023 00:05:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k310-wake-up/m-p/1763502#M28983</guid>
      <dc:creator>hajianik</dc:creator>
      <dc:date>2023-11-25T00:05:58Z</dc:date>
    </item>
  </channel>
</rss>