<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 S32K312EVB-Q172 UART Example not working</title>
    <link>https://community.nxp.com/t5/S32K/S32K312EVB-Q172-UART-Example-not-working/m-p/1762274#M28903</link>
    <description>&lt;P&gt;Hi, S32K3 Team&lt;/P&gt;&lt;P&gt;I can't operate Uart on the board.&lt;/P&gt;&lt;P&gt;Case 1:&lt;/P&gt;&lt;P&gt;&amp;nbsp; I'm trying a 'uart_example_S32K312' with S32K312EVB-Q172.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; Tera term set on Baud Rate,&amp;nbsp; Parity, Stop bit and Word Length, which&amp;nbsp;according to example.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; And&amp;nbsp;UART pins were set on PTD2(gpio[98]) to TX and PTD3 (gpio[99]) to RX to output LPUART_3, which is the basic example setting.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Project builds and debug work.&amp;nbsp;&lt;SPAN&gt;But it doesn't do anything.(Input-not working, Output-not Working)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Case - 2 :&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;Case-1 did not work, so it was set up by changing the Uart channel to 6, Pin Port(PTA16(gpio[16])-TX, PTA-15(gpio[15])-RX)&amp;nbsp; and Interrupt in the example.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;However, an HW Fault has occurred.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; -&amp;nbsp; BusFault: An imprecise (asynchronous) data access error has occurred.&lt;BR /&gt;&amp;nbsp; -&amp;nbsp; HardFault: A fault has been escalated to a hard fault.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Debugging showed that the value was not initialized for the rest of the structures except IP_LPUART_3 in the 'S32K312_LPUART.h' file.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please help me with what I should try.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Installed Software&lt;/P&gt;&lt;P&gt;S32K3 RTD AUTOSAR 4.4 - Version 2.0.0&lt;/P&gt;&lt;P&gt;S32K3xx development package - Version 3.4.3&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regard&lt;/P&gt;</description>
    <pubDate>Thu, 23 Nov 2023 02:04:10 GMT</pubDate>
    <dc:creator>NewbieNerd</dc:creator>
    <dc:date>2023-11-23T02:04:10Z</dc:date>
    <item>
      <title>S32K312EVB-Q172 UART Example not working</title>
      <link>https://community.nxp.com/t5/S32K/S32K312EVB-Q172-UART-Example-not-working/m-p/1762274#M28903</link>
      <description>&lt;P&gt;Hi, S32K3 Team&lt;/P&gt;&lt;P&gt;I can't operate Uart on the board.&lt;/P&gt;&lt;P&gt;Case 1:&lt;/P&gt;&lt;P&gt;&amp;nbsp; I'm trying a 'uart_example_S32K312' with S32K312EVB-Q172.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; Tera term set on Baud Rate,&amp;nbsp; Parity, Stop bit and Word Length, which&amp;nbsp;according to example.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; And&amp;nbsp;UART pins were set on PTD2(gpio[98]) to TX and PTD3 (gpio[99]) to RX to output LPUART_3, which is the basic example setting.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Project builds and debug work.&amp;nbsp;&lt;SPAN&gt;But it doesn't do anything.(Input-not working, Output-not Working)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Case - 2 :&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;Case-1 did not work, so it was set up by changing the Uart channel to 6, Pin Port(PTA16(gpio[16])-TX, PTA-15(gpio[15])-RX)&amp;nbsp; and Interrupt in the example.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;However, an HW Fault has occurred.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; -&amp;nbsp; BusFault: An imprecise (asynchronous) data access error has occurred.&lt;BR /&gt;&amp;nbsp; -&amp;nbsp; HardFault: A fault has been escalated to a hard fault.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Debugging showed that the value was not initialized for the rest of the structures except IP_LPUART_3 in the 'S32K312_LPUART.h' file.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please help me with what I should try.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Installed Software&lt;/P&gt;&lt;P&gt;S32K3 RTD AUTOSAR 4.4 - Version 2.0.0&lt;/P&gt;&lt;P&gt;S32K3xx development package - Version 3.4.3&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regard&lt;/P&gt;</description>
      <pubDate>Thu, 23 Nov 2023 02:04:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312EVB-Q172-UART-Example-not-working/m-p/1762274#M28903</guid>
      <dc:creator>NewbieNerd</dc:creator>
      <dc:date>2023-11-23T02:04:10Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312EVB-Q172 UART Example not working</title>
      <link>https://community.nxp.com/t5/S32K/S32K312EVB-Q172-UART-Example-not-working/m-p/1763049#M28947</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;A1. Please follow the &lt;EM&gt;description.txt&lt;/EM&gt; of &lt;STRONG&gt;Uart_Example_S32K312&lt;/STRONG&gt;:&lt;BR /&gt;&lt;EM&gt;2.2.2 Connections&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;It uses Lpuart instance 3, comunicates with Flexio instance 0 channel 0 for Tx and channel 1 for Rx PTA0(J2.22) - PTD3(J2.10) and PTA1(J2.19) - PTD2(J2.7)&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Uart_Example_S32K312 description.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/251350i56A97E1BF70E9414/image-size/large?v=v2&amp;amp;px=999" role="button" title="Uart_Example_S32K312 description.png" alt="Uart_Example_S32K312 description.png" /&gt;&lt;/span&gt;&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;A2. Please configure the McuPeripheral -&amp;gt;&amp;nbsp;&lt;STRONG&gt;Peripheral Clock Enable&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="McuPeripheral Peripheral Clock Enable.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/251352i8275F4F8072EEEF4/image-size/large?v=v2&amp;amp;px=999" role="button" title="McuPeripheral Peripheral Clock Enable.png" alt="McuPeripheral Peripheral Clock Enable.png" /&gt;&lt;/span&gt;&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="McuPeripheral Peripheral Clock Enable McuPeripheral Peripheral Clock Enable.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/251351i7E40107E436AC4B2/image-size/large?v=v2&amp;amp;px=999" role="button" title="McuPeripheral Peripheral Clock Enable McuPeripheral Peripheral Clock Enable.png" alt="McuPeripheral Peripheral Clock Enable McuPeripheral Peripheral Clock Enable.png" /&gt;&lt;/span&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 24 Nov 2023 05:00:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312EVB-Q172-UART-Example-not-working/m-p/1763049#M28947</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-11-24T05:00:36Z</dc:date>
    </item>
  </channel>
</rss>