<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Can I erase a Phrase (8-byte/64-bit) before program (write) phrase operation for Data Flash in S32K144 ? in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Can-I-erase-a-Phrase-8-byte-64-bit-before-program-write-phrase/m-p/808473#M2887</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/lukaszadrapa"&gt;lukaszadrapa&lt;/A&gt;,&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/jirikral"&gt;jirikral&lt;/A&gt;‌ and&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/danielmartynek"&gt;danielmartynek&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to inform that I am using entire FlexNVM as Data Flash in S32K144 freedom board. I have a application to write only 8-byte in DFlash whenever it's required. For that, I need to erase only 8-byte before write operation. I can write required 8-byte with 'Program Phrase' command available in Flash Driver however I did not find any relative 'Erase Phrase' command for 8-byte erase operation. 'Erase Flash Sector' command does not allow to erase lesser than 2 KB and 'Erase Flash Block' command is erasing entire DFlash of 64 KB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know if it's possible to erase 8-byte only at a time and also if I am not doing it correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You ! :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Jul 2018 12:37:19 GMT</pubDate>
    <dc:creator>nitinverma</dc:creator>
    <dc:date>2018-07-12T12:37:19Z</dc:date>
    <item>
      <title>Can I erase a Phrase (8-byte/64-bit) before program (write) phrase operation for Data Flash in S32K144 ?</title>
      <link>https://community.nxp.com/t5/S32K/Can-I-erase-a-Phrase-8-byte-64-bit-before-program-write-phrase/m-p/808473#M2887</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/lukaszadrapa"&gt;lukaszadrapa&lt;/A&gt;,&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/jirikral"&gt;jirikral&lt;/A&gt;‌ and&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/danielmartynek"&gt;danielmartynek&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to inform that I am using entire FlexNVM as Data Flash in S32K144 freedom board. I have a application to write only 8-byte in DFlash whenever it's required. For that, I need to erase only 8-byte before write operation. I can write required 8-byte with 'Program Phrase' command available in Flash Driver however I did not find any relative 'Erase Phrase' command for 8-byte erase operation. 'Erase Flash Sector' command does not allow to erase lesser than 2 KB and 'Erase Flash Block' command is erasing entire DFlash of 64 KB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know if it's possible to erase 8-byte only at a time and also if I am not doing it correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You ! :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jul 2018 12:37:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-I-erase-a-Phrase-8-byte-64-bit-before-program-write-phrase/m-p/808473#M2887</guid>
      <dc:creator>nitinverma</dc:creator>
      <dc:date>2018-07-12T12:37:19Z</dc:date>
    </item>
    <item>
      <title>Re: Can I erase a Phrase (8-byte/64-bit) before program (write) phrase operation for Data Flash in S32K144 ?</title>
      <link>https://community.nxp.com/t5/S32K/Can-I-erase-a-Phrase-8-byte-64-bit-before-program-write-phrase/m-p/808474#M2888</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Nitin,&lt;/P&gt;&lt;P&gt;Unfortunately, this is not possible.&lt;/P&gt;&lt;P&gt;The smallest portion of D-Flash that can be erased is the 2K sector.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jul 2018 12:41:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-I-erase-a-Phrase-8-byte-64-bit-before-program-write-phrase/m-p/808474#M2888</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-07-12T12:41:28Z</dc:date>
    </item>
    <item>
      <title>Re: Can I erase a Phrase (8-byte/64-bit) before program (write) phrase operation for Data Flash in S32K144 ?</title>
      <link>https://community.nxp.com/t5/S32K/Can-I-erase-a-Phrase-8-byte-64-bit-before-program-write-phrase/m-p/808475#M2889</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;:smileysad:. Anyways thanks a lot Daniel for your prompt response.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jul 2018 13:03:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Can-I-erase-a-Phrase-8-byte-64-bit-before-program-write-phrase/m-p/808475#M2889</guid>
      <dc:creator>nitinverma</dc:creator>
      <dc:date>2018-07-12T13:03:30Z</dc:date>
    </item>
  </channel>
</rss>