<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Trigger sources for ADC in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Trigger-sources-for-ADC/m-p/1760061#M28786</link>
    <description>&lt;P&gt;I want to generate ADC drivers for S32K344 using S32DS IDE for non-autosar. After going through the RM I have understood that there is a hardware trigger for conversion using the TRGMUX. Instead, for normal conversion mode, is there a way to trigger the ADC conversion periodically (with a timer). Is there any configuration to do this inside the ADC configurations in the code generator itself.&lt;/P&gt;</description>
    <pubDate>Mon, 20 Nov 2023 20:04:13 GMT</pubDate>
    <dc:creator>enthuCutlet</dc:creator>
    <dc:date>2023-11-20T20:04:13Z</dc:date>
    <item>
      <title>Trigger sources for ADC</title>
      <link>https://community.nxp.com/t5/S32K/Trigger-sources-for-ADC/m-p/1760061#M28786</link>
      <description>&lt;P&gt;I want to generate ADC drivers for S32K344 using S32DS IDE for non-autosar. After going through the RM I have understood that there is a hardware trigger for conversion using the TRGMUX. Instead, for normal conversion mode, is there a way to trigger the ADC conversion periodically (with a timer). Is there any configuration to do this inside the ADC configurations in the code generator itself.&lt;/P&gt;</description>
      <pubDate>Mon, 20 Nov 2023 20:04:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Trigger-sources-for-ADC/m-p/1760061#M28786</guid>
      <dc:creator>enthuCutlet</dc:creator>
      <dc:date>2023-11-20T20:04:13Z</dc:date>
    </item>
    <item>
      <title>Re: Trigger sources for ADC</title>
      <link>https://community.nxp.com/t5/S32K/Trigger-sources-for-ADC/m-p/1760144#M28789</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please refer to:&amp;nbsp;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-PIT-BTCU-parallel-ADC-FIFO-DMA-DS3-5-RTD300/ta-p/1732444" target="_self"&gt;Example S32K344 PIT BTCU parallel ADC FIFO DMA DS3.5 RTD300&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-PIT-BTCU-ADC-DMA-DS3-4-RTD100/ta-p/1435324" target="_self"&gt;Example S32K344 PIT BTCU ADC DMA DS3.4 RTD100&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 21 Nov 2023 00:43:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Trigger-sources-for-ADC/m-p/1760144#M28789</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-11-21T00:43:53Z</dc:date>
    </item>
    <item>
      <title>Re: Trigger sources for ADC</title>
      <link>https://community.nxp.com/t5/S32K/Trigger-sources-for-ADC/m-p/1760360#M28797</link>
      <description>&lt;P&gt;Is there an example without using BCTU. Instead using a periodic interrupt for Normal conversion mode&lt;/P&gt;</description>
      <pubDate>Tue, 21 Nov 2023 05:02:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Trigger-sources-for-ADC/m-p/1760360#M28797</guid>
      <dc:creator>enthuCutlet</dc:creator>
      <dc:date>2023-11-21T05:02:12Z</dc:date>
    </item>
    <item>
      <title>Re: Trigger sources for ADC</title>
      <link>https://community.nxp.com/t5/S32K/Trigger-sources-for-ADC/m-p/1760362#M28798</link>
      <description>Is there an example without using BCTU. Instead using a periodic interrupt for Normal conversion mode</description>
      <pubDate>Tue, 21 Nov 2023 05:02:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Trigger-sources-for-ADC/m-p/1760362#M28798</guid>
      <dc:creator>enthuCutlet</dc:creator>
      <dc:date>2023-11-21T05:02:54Z</dc:date>
    </item>
  </channel>
</rss>