<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 S32K311 LPSPI Master Mode not working</title>
    <link>https://community.nxp.com/t5/S32K/S32K311-LPSPI-Master-Mode-not-working/m-p/1757388#M28651</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I tried to communicate with LPSPI, but it doesn't work.&lt;/P&gt;&lt;P&gt;I use RTD and its parameters are set with EB Tresos.&lt;BR /&gt;The attached files are the parameters for SPI Driver.&lt;/P&gt;&lt;P&gt;In my source code, I call the functions, Spi_SetupEB() and&amp;nbsp;Spi_AsyncTransmit().&lt;BR /&gt;&lt;SPAN&gt;Then the interruption occurs and LPSPI SR register suggests the transmission completes, however, any data is not received nor sent.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;In the oscilloscope waves, SIN, SOUT, SCLK, and CS keep low level.&lt;/P&gt;&lt;P&gt;Is there something missing from my setting for RTD?&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Could you give me some advice?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
    <pubDate>Wed, 15 Nov 2023 07:35:03 GMT</pubDate>
    <dc:creator>MickMick</dc:creator>
    <dc:date>2023-11-15T07:35:03Z</dc:date>
    <item>
      <title>S32K311 LPSPI Master Mode not working</title>
      <link>https://community.nxp.com/t5/S32K/S32K311-LPSPI-Master-Mode-not-working/m-p/1757388#M28651</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I tried to communicate with LPSPI, but it doesn't work.&lt;/P&gt;&lt;P&gt;I use RTD and its parameters are set with EB Tresos.&lt;BR /&gt;The attached files are the parameters for SPI Driver.&lt;/P&gt;&lt;P&gt;In my source code, I call the functions, Spi_SetupEB() and&amp;nbsp;Spi_AsyncTransmit().&lt;BR /&gt;&lt;SPAN&gt;Then the interruption occurs and LPSPI SR register suggests the transmission completes, however, any data is not received nor sent.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;In the oscilloscope waves, SIN, SOUT, SCLK, and CS keep low level.&lt;/P&gt;&lt;P&gt;Is there something missing from my setting for RTD?&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Could you give me some advice?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Wed, 15 Nov 2023 07:35:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K311-LPSPI-Master-Mode-not-working/m-p/1757388#M28651</guid>
      <dc:creator>MickMick</dc:creator>
      <dc:date>2023-11-15T07:35:03Z</dc:date>
    </item>
    <item>
      <title>Re: S32K311 LPSPI Master Mode not working</title>
      <link>https://community.nxp.com/t5/S32K/S32K311-LPSPI-Master-Mode-not-working/m-p/1761622#M28854</link>
      <description>&lt;P&gt;Did you config for Pin and Port module for SPI's pins ?&lt;BR /&gt;We provided examples for EB Tresos and S32DS for SPI module in installed package already, you can consider it as a reference:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="cuongnguyenphu_0-1700635078885.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/251020i4E6AC0245650651F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="cuongnguyenphu_0-1700635078885.png" alt="cuongnguyenphu_0-1700635078885.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;cuongnguyenphu_0-1700635078885.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 22 Nov 2023 06:38:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K311-LPSPI-Master-Mode-not-working/m-p/1761622#M28854</guid>
      <dc:creator>cuongnguyenphu</dc:creator>
      <dc:date>2023-11-22T06:38:14Z</dc:date>
    </item>
    <item>
      <title>Re: S32K311 LPSPI Master Mode not working</title>
      <link>https://community.nxp.com/t5/S32K/S32K311-LPSPI-Master-Mode-not-working/m-p/1761697#M28861</link>
      <description>&lt;P&gt;I checked the port settings and realized that the sss setting was incorrect.&lt;/P&gt;&lt;P&gt;Thank you very much!&lt;/P&gt;</description>
      <pubDate>Wed, 22 Nov 2023 07:53:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K311-LPSPI-Master-Mode-not-working/m-p/1761697#M28861</guid>
      <dc:creator>MickMick</dc:creator>
      <dc:date>2023-11-22T07:53:20Z</dc:date>
    </item>
  </channel>
</rss>