<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K146 CAN</title>
    <link>https://community.nxp.com/t5/S32K/S32K146-CAN/m-p/1757269#M28641</link>
    <description>&lt;P&gt;&lt;A href="mailto:Hi@mahesh09" target="_blank"&gt;Hi@mahesh09&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;1."&lt;SPAN&gt;User manual states, when a message is transmitted, IFLAG of the corresponding message object will get set. Is this the case for remote frame as well?&lt;/SPAN&gt;"&lt;/P&gt;
&lt;P&gt;yes, a status flag is set in the Interrupt Flag register and an interrupt is generated if allowed by the corresponding Interrupt Mask Register bit.&lt;/P&gt;
&lt;P&gt;2. "&lt;SPAN&gt;well? If so, is there a chance software can copy incorrect data from message buffer as IFLAG is already set?&lt;/SPAN&gt;"&lt;/P&gt;
&lt;P&gt;for your sentence, I guess you're refer to Receive Process right?&lt;/P&gt;
&lt;P&gt;if yes, you can take a look at the S32K-RM,FlexCAN-&amp;gt;Receive Process.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_0-1700016796942.png" style="width: 707px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/249822iBB4F6B3085BF45BF/image-dimensions/707x242?v=v2" width="707" height="242" role="button" title="Senlent_0-1700016796942.png" alt="Senlent_0-1700016796942.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Senlent_0-1700016796942.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 15 Nov 2023 02:58:39 GMT</pubDate>
    <dc:creator>Senlent</dc:creator>
    <dc:date>2023-11-15T02:58:39Z</dc:date>
    <item>
      <title>S32K146 CAN</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-CAN/m-p/1757036#M28634</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;I am using FLEXCAN in S32K146. 4 CAN messages are received using remote frame concept. Out of 4 messages, the first message data is filled with zeroes and correct data is received for the remaining 3 messages.&lt;/P&gt;&lt;P&gt;Below procedure is followed:&lt;BR /&gt;Send remote frame requesting 4 CAN messages.&lt;BR /&gt;Software keeps polling IFLAG register to see which CAN message is received. If IFLAG of corresponding message is set, data is copied from MB.&lt;/P&gt;&lt;P&gt;User manual states, when a message is transmitted, IFLAG of the corresponding message object will get set. Is this the case for remote frame as well? If so, is there a chance software can copy incorrect data from message buffer as IFLAG is already set?&lt;BR /&gt;NOTE: Polling of CODE filed of message object is not recommended in user manual. If CODE field is also checked along with IFLAG then it is giving a different issue.&lt;/P&gt;</description>
      <pubDate>Tue, 14 Nov 2023 16:24:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-CAN/m-p/1757036#M28634</guid>
      <dc:creator>mahesh09</dc:creator>
      <dc:date>2023-11-14T16:24:56Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 CAN</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-CAN/m-p/1757269#M28641</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@mahesh09" target="_blank"&gt;Hi@mahesh09&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;1."&lt;SPAN&gt;User manual states, when a message is transmitted, IFLAG of the corresponding message object will get set. Is this the case for remote frame as well?&lt;/SPAN&gt;"&lt;/P&gt;
&lt;P&gt;yes, a status flag is set in the Interrupt Flag register and an interrupt is generated if allowed by the corresponding Interrupt Mask Register bit.&lt;/P&gt;
&lt;P&gt;2. "&lt;SPAN&gt;well? If so, is there a chance software can copy incorrect data from message buffer as IFLAG is already set?&lt;/SPAN&gt;"&lt;/P&gt;
&lt;P&gt;for your sentence, I guess you're refer to Receive Process right?&lt;/P&gt;
&lt;P&gt;if yes, you can take a look at the S32K-RM,FlexCAN-&amp;gt;Receive Process.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_0-1700016796942.png" style="width: 707px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/249822iBB4F6B3085BF45BF/image-dimensions/707x242?v=v2" width="707" height="242" role="button" title="Senlent_0-1700016796942.png" alt="Senlent_0-1700016796942.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Senlent_0-1700016796942.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Nov 2023 02:58:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-CAN/m-p/1757269#M28641</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2023-11-15T02:58:39Z</dc:date>
    </item>
  </channel>
</rss>