<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K148 FlexRAM Question in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K148-FlexRAM-Question/m-p/1756086#M28583</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1.&lt;/P&gt;&lt;P&gt;I need to know the value of FlexRAM area when it is delivered from NXP (Virgin Device)&lt;/P&gt;&lt;P&gt;[0x14000000 ~&amp;nbsp;0x1400ffff]&lt;/P&gt;&lt;P&gt;Currently, I don't have the s32k148 virgin device. So I can't check the value.&lt;/P&gt;&lt;P&gt;(Random(garbage) Value or 0 or 1?)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2.&lt;/P&gt;&lt;P&gt;I have develepment board.&lt;/P&gt;&lt;P&gt;And I did "partition command" to this EVB for csec use.&lt;/P&gt;&lt;P&gt;And after I did "erase all command" to this EVB, FlexRAM area value became 0xFF.&lt;/P&gt;&lt;P&gt;Is this value moved from FlexNVM?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;These are related to mass production project.&lt;/P&gt;&lt;P&gt;I'm looking forward to reply.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Phillip&lt;/P&gt;</description>
    <pubDate>Mon, 13 Nov 2023 07:42:33 GMT</pubDate>
    <dc:creator>kmh48301</dc:creator>
    <dc:date>2023-11-13T07:42:33Z</dc:date>
    <item>
      <title>S32K148 FlexRAM Question</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-FlexRAM-Question/m-p/1756086#M28583</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1.&lt;/P&gt;&lt;P&gt;I need to know the value of FlexRAM area when it is delivered from NXP (Virgin Device)&lt;/P&gt;&lt;P&gt;[0x14000000 ~&amp;nbsp;0x1400ffff]&lt;/P&gt;&lt;P&gt;Currently, I don't have the s32k148 virgin device. So I can't check the value.&lt;/P&gt;&lt;P&gt;(Random(garbage) Value or 0 or 1?)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2.&lt;/P&gt;&lt;P&gt;I have develepment board.&lt;/P&gt;&lt;P&gt;And I did "partition command" to this EVB for csec use.&lt;/P&gt;&lt;P&gt;And after I did "erase all command" to this EVB, FlexRAM area value became 0xFF.&lt;/P&gt;&lt;P&gt;Is this value moved from FlexNVM?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;These are related to mass production project.&lt;/P&gt;&lt;P&gt;I'm looking forward to reply.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Phillip&lt;/P&gt;</description>
      <pubDate>Mon, 13 Nov 2023 07:42:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-FlexRAM-Question/m-p/1756086#M28583</guid>
      <dc:creator>kmh48301</dc:creator>
      <dc:date>2023-11-13T07:42:33Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148 FlexRAM Question</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-FlexRAM-Question/m-p/1758223#M28694</link>
      <description>&lt;P&gt;I the past I made example code for this:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K146-Set-whole-FlexRAM-as-RAM-v0-0-S32DS-ARM-2-2/ta-p/1245841" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K146-Set-whole-FlexRAM-as-RAM-v0-0-S32DS-ARM-2-2/ta-p/1245841&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Pay attention to its description&lt;/P&gt;</description>
      <pubDate>Thu, 16 Nov 2023 08:45:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-FlexRAM-Question/m-p/1758223#M28694</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2023-11-16T08:45:03Z</dc:date>
    </item>
  </channel>
</rss>