<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K344 dual core and bootloader in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K344-dual-core-and-bootloader/m-p/1754011#M28478</link>
    <description>&lt;P&gt;Hello. Thank you for your reply. The bootloader works properly (I think ) ). The problem exists when I link one of the tasks to core 1. In case all tasks are linked to core 0, everything works fine. Points where cores stuck are attached.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="esmax_0-1699439670789.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/249002i49A3004C50F0F549/image-size/medium?v=v2&amp;amp;px=400" role="button" title="esmax_0-1699439670789.png" alt="esmax_0-1699439670789.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;esmax_0-1699439670789.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="esmax_1-1699439698123.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/249003i6BC0A2726F991319/image-size/medium?v=v2&amp;amp;px=400" role="button" title="esmax_1-1699439698123.png" alt="esmax_1-1699439698123.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;esmax_1-1699439698123.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 08 Nov 2023 10:35:09 GMT</pubDate>
    <dc:creator>esmax</dc:creator>
    <dc:date>2023-11-08T10:35:09Z</dc:date>
    <item>
      <title>S32K344 dual core and bootloader</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-dual-core-and-bootloader/m-p/1753657#M28467</link>
      <description>&lt;P&gt;Hello, I have a project based on S32K324. Cores are decoupled. The application flashed via bootloader is not working.&amp;nbsp;Core 0 waits for X-signal and core 1 gets stuck in BswM_CoreSync. What can be a problem? Thank you in advance.&lt;/P&gt;</description>
      <pubDate>Tue, 07 Nov 2023 18:07:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-dual-core-and-bootloader/m-p/1753657#M28467</guid>
      <dc:creator>esmax</dc:creator>
      <dc:date>2023-11-07T18:07:13Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 dual core and bootloader</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-dual-core-and-bootloader/m-p/1753983#M28475</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/211053"&gt;@esmax&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;is everything completely de-initialized before jumping from bootloader to the application? Are interrupts disabled? I mean on all levels - in the core, NVIC, local enable bits in peripherals. This is the most common problem.&lt;/P&gt;
&lt;P&gt;Did you try to dump the flash memory and compare it with original binary to see if the application is programmed correctly?&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Wed, 08 Nov 2023 07:12:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-dual-core-and-bootloader/m-p/1753983#M28475</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2023-11-08T07:12:34Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 dual core and bootloader</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-dual-core-and-bootloader/m-p/1754011#M28478</link>
      <description>&lt;P&gt;Hello. Thank you for your reply. The bootloader works properly (I think ) ). The problem exists when I link one of the tasks to core 1. In case all tasks are linked to core 0, everything works fine. Points where cores stuck are attached.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="esmax_0-1699439670789.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/249002i49A3004C50F0F549/image-size/medium?v=v2&amp;amp;px=400" role="button" title="esmax_0-1699439670789.png" alt="esmax_0-1699439670789.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;esmax_0-1699439670789.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="esmax_1-1699439698123.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/249003i6BC0A2726F991319/image-size/medium?v=v2&amp;amp;px=400" role="button" title="esmax_1-1699439698123.png" alt="esmax_1-1699439698123.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;esmax_1-1699439698123.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 08 Nov 2023 10:35:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-dual-core-and-bootloader/m-p/1754011#M28478</guid>
      <dc:creator>esmax</dc:creator>
      <dc:date>2023-11-08T10:35:09Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 dual core and bootloader</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-dual-core-and-bootloader/m-p/1757584#M28666</link>
      <description>&lt;P&gt;The problem was in the configuration of&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;IRSPRC0 register.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Wed, 15 Nov 2023 10:55:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-dual-core-and-bootloader/m-p/1757584#M28666</guid>
      <dc:creator>esmax</dc:creator>
      <dc:date>2023-11-15T10:55:56Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 dual core and bootloader</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-dual-core-and-bootloader/m-p/1851295#M34470</link>
      <description>&lt;P&gt;Hi, I am using the project "S32K344_Can_bootloader_RTD200" in the microprocessor S32K344. I want to download an application with the program of bootloader. I have achieved the jump from program to application but I have different questions. 1. I want to use #define EN_DELAY_TIME but when I uncomment the command in the folder "public_in", the program has different errors. My target to use "Backdoor", that is to say, I want to check if the program has to enter to bootloader or not. I don´t know the process and the different functions that I have to use to achieve the target. I want to use the function "Boot_CheckReqBootloaderMode(void)" but when I debug the program, it never enters to the "if". Could you explain me the process and the steps to achieve the target. I add different functions that I think are important. 2. I don´t know if I have to modificate the parameters of "static tJumpAppDelayTimeInfo gs_stJumpAPPDelayTimeInfo = {FALSE, 0u};". I have to change this structure ? You can see all structure in one of the next pictures. I need the reply as soon as possible since I have to send a project very soon.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JonAnder_Amante_0-1713768071250.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/274893iE0D2622957BE5F47/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JonAnder_Amante_0-1713768071250.png" alt="JonAnder_Amante_0-1713768071250.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;JonAnder_Amante_0-1713768071250.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JonAnder_Amante_1-1713768071252.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/274894i313242E2346DAC27/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JonAnder_Amante_1-1713768071252.png" alt="JonAnder_Amante_1-1713768071252.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;JonAnder_Amante_1-1713768071252.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JonAnder_Amante_2-1713768071254.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/274895i4D91DBF66F33EB63/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JonAnder_Amante_2-1713768071254.png" alt="JonAnder_Amante_2-1713768071254.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;JonAnder_Amante_2-1713768071254.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JonAnder_Amante_3-1713768071257.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/274896i6E12D527351FF4F4/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JonAnder_Amante_3-1713768071257.png" alt="JonAnder_Amante_3-1713768071257.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;JonAnder_Amante_3-1713768071257.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JonAnder_Amante_4-1713768071256.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/274897iB5202DD3245503C8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JonAnder_Amante_4-1713768071256.png" alt="JonAnder_Amante_4-1713768071256.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;JonAnder_Amante_4-1713768071256.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for all,&lt;/P&gt;</description>
      <pubDate>Mon, 22 Apr 2024 06:41:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-dual-core-and-bootloader/m-p/1851295#M34470</guid>
      <dc:creator>JonAnder_Amante</dc:creator>
      <dc:date>2024-04-22T06:41:27Z</dc:date>
    </item>
  </channel>
</rss>