<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Need help to set Rx FIFO configuration for CAN instance 1 and instance 2 for S32K3xx in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Need-help-to-set-Rx-FIFO-configuration-for-CAN-instance-1-and/m-p/1752825#M28426</link>
    <description>&lt;P&gt;Hello BR, Petr ,&lt;/P&gt;&lt;P&gt;If possible can you suggest solution to achieve below requirement&lt;/P&gt;&lt;P&gt;&amp;gt;configure HW filters with CAN-FD.&lt;/P&gt;&lt;P&gt;&amp;nbsp;I m using S32K344&lt;/P&gt;</description>
    <pubDate>Mon, 06 Nov 2023 12:15:01 GMT</pubDate>
    <dc:creator>marotib</dc:creator>
    <dc:date>2023-11-06T12:15:01Z</dc:date>
    <item>
      <title>Need help to set Rx FIFO configuration for CAN instance 1 and instance 2 for S32K3xx</title>
      <link>https://community.nxp.com/t5/S32K/Need-help-to-set-Rx-FIFO-configuration-for-CAN-instance-1-and/m-p/1752659#M28417</link>
      <description>&lt;P&gt;Currently in my project :&amp;nbsp;&amp;nbsp;CAN Instance 0 is used for DAQ in normal mode ,CAN Instance 1 is used for PTCAN in normal mode and CAN instance 2 is used for PTCAN in listen only mode.&lt;/P&gt;&lt;P&gt;Now we are able to set CAN HW filters on CAN_0 and everything working as expected but we are unable to set CAN HW filters on instance CAN_1 and CAN_2.&lt;/P&gt;&lt;P&gt;In configuration tool --&amp;gt; enhanced rxfifo configuration option is disable for both the instance 1 &amp;amp; 2 and If I try to do the same through software then init getting fail.&lt;/P&gt;&lt;P&gt;So please let me know the way to set enhanced rxfifo.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 06 Nov 2023 08:50:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Need-help-to-set-Rx-FIFO-configuration-for-CAN-instance-1-and/m-p/1752659#M28417</guid>
      <dc:creator>marotib</dc:creator>
      <dc:date>2023-11-06T08:50:21Z</dc:date>
    </item>
    <item>
      <title>Re: Need help to set Rx FIFO configuration for CAN instance 1 and instance 2 for S32K3xx</title>
      <link>https://community.nxp.com/t5/S32K/Need-help-to-set-Rx-FIFO-configuration-for-CAN-instance-1-and/m-p/1752801#M28425</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;you did not specify a device, but most probably an Enhanced RXFIFO is not available for used instances.&lt;BR /&gt;Refer to chapter&amp;nbsp;74.1 Chip-specific FlexCAN information of the device RM for implementation.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Mon, 06 Nov 2023 11:39:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Need-help-to-set-Rx-FIFO-configuration-for-CAN-instance-1-and/m-p/1752801#M28425</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-11-06T11:39:47Z</dc:date>
    </item>
    <item>
      <title>Re: Need help to set Rx FIFO configuration for CAN instance 1 and instance 2 for S32K3xx</title>
      <link>https://community.nxp.com/t5/S32K/Need-help-to-set-Rx-FIFO-configuration-for-CAN-instance-1-and/m-p/1752825#M28426</link>
      <description>&lt;P&gt;Hello BR, Petr ,&lt;/P&gt;&lt;P&gt;If possible can you suggest solution to achieve below requirement&lt;/P&gt;&lt;P&gt;&amp;gt;configure HW filters with CAN-FD.&lt;/P&gt;&lt;P&gt;&amp;nbsp;I m using S32K344&lt;/P&gt;</description>
      <pubDate>Mon, 06 Nov 2023 12:15:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Need-help-to-set-Rx-FIFO-configuration-for-CAN-instance-1-and/m-p/1752825#M28426</guid>
      <dc:creator>marotib</dc:creator>
      <dc:date>2023-11-06T12:15:01Z</dc:date>
    </item>
    <item>
      <title>Re: Need help to set Rx FIFO configuration for CAN instance 1 and instance 2 for S32K3xx</title>
      <link>https://community.nxp.com/t5/S32K/Need-help-to-set-Rx-FIFO-configuration-for-CAN-instance-1-and/m-p/1752826#M28427</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;for enhanced RXFIFO example you can refer to&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-test-S32DS3-4/ta-p/1536225" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-test-S32DS3-4/ta-p/1536225&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Mon, 06 Nov 2023 12:24:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Need-help-to-set-Rx-FIFO-configuration-for-CAN-instance-1-and/m-p/1752826#M28427</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-11-06T12:24:16Z</dc:date>
    </item>
  </channel>
</rss>