<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K series MCU VOL Level in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K-series-MCU-VOL-Level/m-p/1752009#M28398</link>
    <description>&lt;P&gt;Dear Team,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Could you please support us to get an answer for the below question.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1.&amp;nbsp;&lt;/SPAN&gt;&lt;FONT color="#0000ff"&gt;What is the Digital output Low (VOL) for this MCU?&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#000000"&gt;&lt;SPAN&gt;GPIO output from the MCU is connected to an IC which is expecting input voltage less than 0.5V to detect the Low level.&amp;nbsp;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;DIV&gt;I could see in the S32K series datasheet that the VOL voltage is mentioned as&amp;nbsp;VOL &amp;lt;= 0.7V which is the Maximum Value.&lt;/DIV&gt;&lt;DIV&gt;I understand that the&amp;nbsp;actual&amp;nbsp;VOL will be dependent on the current draw and the type of pin being used (Standard, Standard-Plus, Medium, Fast).&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;I Am not sure how to ensure the VOL (MCU) is less than the VIL max of other devices.&lt;/DIV&gt;&lt;DIV&gt;Is it right to consider it as a Linear function and take the Actual VOL value using below formula&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT color="#0000FF"&gt;VOL (MCU) = (Actual Current per Pin / Rated Current of each Pin) x VOL Max.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;Considering VOL Max = 0.7V.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards&lt;/DIV&gt;&lt;DIV&gt;Sreelakshmi A&lt;/DIV&gt;&lt;/DIV&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 03 Nov 2023 13:13:26 GMT</pubDate>
    <dc:creator>Sreelakshmi</dc:creator>
    <dc:date>2023-11-03T13:13:26Z</dc:date>
    <item>
      <title>S32K series MCU VOL Level</title>
      <link>https://community.nxp.com/t5/S32K/S32K-series-MCU-VOL-Level/m-p/1752009#M28398</link>
      <description>&lt;P&gt;Dear Team,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Could you please support us to get an answer for the below question.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1.&amp;nbsp;&lt;/SPAN&gt;&lt;FONT color="#0000ff"&gt;What is the Digital output Low (VOL) for this MCU?&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#000000"&gt;&lt;SPAN&gt;GPIO output from the MCU is connected to an IC which is expecting input voltage less than 0.5V to detect the Low level.&amp;nbsp;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;DIV&gt;I could see in the S32K series datasheet that the VOL voltage is mentioned as&amp;nbsp;VOL &amp;lt;= 0.7V which is the Maximum Value.&lt;/DIV&gt;&lt;DIV&gt;I understand that the&amp;nbsp;actual&amp;nbsp;VOL will be dependent on the current draw and the type of pin being used (Standard, Standard-Plus, Medium, Fast).&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;I Am not sure how to ensure the VOL (MCU) is less than the VIL max of other devices.&lt;/DIV&gt;&lt;DIV&gt;Is it right to consider it as a Linear function and take the Actual VOL value using below formula&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT color="#0000FF"&gt;VOL (MCU) = (Actual Current per Pin / Rated Current of each Pin) x VOL Max.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;Considering VOL Max = 0.7V.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards&lt;/DIV&gt;&lt;DIV&gt;Sreelakshmi A&lt;/DIV&gt;&lt;/DIV&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 03 Nov 2023 13:13:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-series-MCU-VOL-Level/m-p/1752009#M28398</guid>
      <dc:creator>Sreelakshmi</dc:creator>
      <dc:date>2023-11-03T13:13:26Z</dc:date>
    </item>
    <item>
      <title>Re: S32K series MCU VOL Level</title>
      <link>https://community.nxp.com/t5/S32K/S32K-series-MCU-VOL-Level/m-p/1752282#M28406</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/225269"&gt;@Sreelakshmi&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;At low currents, the characteristic is more or less liner.&lt;/P&gt;
&lt;P&gt;Refer to&amp;nbsp;AN2434 Input/Output (I/O) Pin Drivers on HCS12 Family MCUs.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN2434.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN2434.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1699097033104.png" style="width: 572px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/248473i0D7166F86825FAB9/image-dimensions/572x409?v=v2" width="572" height="409" role="button" title="danielmartynek_0-1699097033104.png" alt="danielmartynek_0-1699097033104.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 04 Nov 2023 11:25:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-series-MCU-VOL-Level/m-p/1752282#M28406</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2023-11-04T11:25:41Z</dc:date>
    </item>
  </channel>
</rss>