<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Disable Multi-Bit ECC Error Exception</title>
    <link>https://community.nxp.com/t5/S32K/Disable-Multi-Bit-ECC-Error-Exception/m-p/1750954#M28359</link>
    <description>&lt;P&gt;Hello everyone, when I used UDSboot to test the update program, a Multi-Bit ECC Error occurred, which caused the program to get stuck in the hardware fault handler and could not update the program again through UDSboot. Then I configured PFCR[DMEEE] to 1, which could solve the problem of getting stuck. I wonder if the official advice is to Disable Multi-Bit ECC Error Exception?&lt;/P&gt;</description>
    <pubDate>Thu, 02 Nov 2023 08:38:25 GMT</pubDate>
    <dc:creator>paul_jack</dc:creator>
    <dc:date>2023-11-02T08:38:25Z</dc:date>
    <item>
      <title>Disable Multi-Bit ECC Error Exception</title>
      <link>https://community.nxp.com/t5/S32K/Disable-Multi-Bit-ECC-Error-Exception/m-p/1750954#M28359</link>
      <description>&lt;P&gt;Hello everyone, when I used UDSboot to test the update program, a Multi-Bit ECC Error occurred, which caused the program to get stuck in the hardware fault handler and could not update the program again through UDSboot. Then I configured PFCR[DMEEE] to 1, which could solve the problem of getting stuck. I wonder if the official advice is to Disable Multi-Bit ECC Error Exception?&lt;/P&gt;</description>
      <pubDate>Thu, 02 Nov 2023 08:38:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Disable-Multi-Bit-ECC-Error-Exception/m-p/1750954#M28359</guid>
      <dc:creator>paul_jack</dc:creator>
      <dc:date>2023-11-02T08:38:25Z</dc:date>
    </item>
  </channel>
</rss>