<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Unified Bootloader Flow Control Issue in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Unified-Bootloader-Flow-Control-Issue/m-p/1749373#M28270</link>
    <description>&lt;P&gt;Dear Sir/Ma'am,&lt;/P&gt;&lt;P&gt;PFA Log &amp;amp; functions&lt;/P&gt;&lt;P&gt;I'm working on UDS using unified_bootloader_demo_v2.1. I'm using S32K146 controller.&lt;BR /&gt;&lt;BR /&gt;library porting &amp;amp; integration was successful I was able to test services such as session control, read &amp;amp; write data by identifier.&amp;nbsp;&lt;BR /&gt;but when I tried to execute security access service. following happened&lt;BR /&gt;1)security access request&amp;nbsp; sent using GUI/UI "NXP Open Bus" or "ECU Bus".&lt;/P&gt;&lt;P&gt;2)First frame received from the hardware.&lt;/P&gt;&lt;P&gt;then UI/GUI didn't send the Flow control frame.&lt;BR /&gt;&lt;BR /&gt;also I would like to understand how to use can_tp.c functions for receiving &amp;amp; transmitting first frame, flow control frame, consecutive frame etc. does TP maintains the status if transmitted data is more than 8 bytes?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Pratik&lt;/P&gt;</description>
    <pubDate>Tue, 31 Oct 2023 09:17:50 GMT</pubDate>
    <dc:creator>pratikkul26</dc:creator>
    <dc:date>2023-10-31T09:17:50Z</dc:date>
    <item>
      <title>Unified Bootloader Flow Control Issue</title>
      <link>https://community.nxp.com/t5/S32K/Unified-Bootloader-Flow-Control-Issue/m-p/1749373#M28270</link>
      <description>&lt;P&gt;Dear Sir/Ma'am,&lt;/P&gt;&lt;P&gt;PFA Log &amp;amp; functions&lt;/P&gt;&lt;P&gt;I'm working on UDS using unified_bootloader_demo_v2.1. I'm using S32K146 controller.&lt;BR /&gt;&lt;BR /&gt;library porting &amp;amp; integration was successful I was able to test services such as session control, read &amp;amp; write data by identifier.&amp;nbsp;&lt;BR /&gt;but when I tried to execute security access service. following happened&lt;BR /&gt;1)security access request&amp;nbsp; sent using GUI/UI "NXP Open Bus" or "ECU Bus".&lt;/P&gt;&lt;P&gt;2)First frame received from the hardware.&lt;/P&gt;&lt;P&gt;then UI/GUI didn't send the Flow control frame.&lt;BR /&gt;&lt;BR /&gt;also I would like to understand how to use can_tp.c functions for receiving &amp;amp; transmitting first frame, flow control frame, consecutive frame etc. does TP maintains the status if transmitted data is more than 8 bytes?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Pratik&lt;/P&gt;</description>
      <pubDate>Tue, 31 Oct 2023 09:17:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unified-Bootloader-Flow-Control-Issue/m-p/1749373#M28270</guid>
      <dc:creator>pratikkul26</dc:creator>
      <dc:date>2023-10-31T09:17:50Z</dc:date>
    </item>
  </channel>
</rss>