<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Write fail between two sectors with same cluster in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Write-fail-between-two-sectors-with-same-cluster/m-p/1739960#M27851</link>
    <description>&lt;P&gt;This thread is duplicated with below thread:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K/Fls-module-return-a-error-length-when-Fee-block-data-through-two/td-p/1713047" target="_blank"&gt;https://community.nxp.com/t5/S32K/Fls-module-return-a-error-length-when-Fee-block-data-through-two/td-p/1713047&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 16 Oct 2023 04:06:10 GMT</pubDate>
    <dc:creator>cuongnguyenphu</dc:creator>
    <dc:date>2023-10-16T04:06:10Z</dc:date>
    <item>
      <title>Write fail between two sectors with same cluster</title>
      <link>https://community.nxp.com/t5/S32K/Write-fail-between-two-sectors-with-same-cluster/m-p/1714985#M26666</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We meet an issue when use Fls function with "&lt;SPAN&gt;&lt;SPAN class=""&gt;Fls_TS_T40D2M10I1R0&lt;/SPAN&gt;&lt;/SPAN&gt;" on S32K146. The process is below:&lt;/P&gt;&lt;P&gt;1. Set 2K for each sector, such as sector 0, 1, 2, 3, an so on&lt;/P&gt;&lt;P&gt;2. Config Sector 0, 1, 2, 3, 4 to cluster0&lt;/P&gt;&lt;P&gt;3.&amp;nbsp;Config Sector 5, 6, 7, 8, 9 to cluster1&lt;/P&gt;&lt;P&gt;4. Config cluster0 and cluster1 to ClusterGroupAPP&lt;/P&gt;&lt;P&gt;4. Config blocks inside of Cluster GroupAPP. one of the blocks occupy 208bytes&lt;/P&gt;&lt;P&gt;We found sometimes code will run to the branch below and write will stop when try to write from sector 3 to sector 4 like the picture below. The address 0x1000 D000 is the boundary for sector3 and sector4.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="charles_wangw_0-1693478392112.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/239070i4DA6C83841E0D695/image-size/medium?v=v2&amp;amp;px=400" role="button" title="charles_wangw_0-1693478392112.png" alt="charles_wangw_0-1693478392112.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;charles_wangw_0-1693478392112.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="charles_wangw_1-1693478613716.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/239071i8B03EF2CA74C5D53/image-size/medium?v=v2&amp;amp;px=400" role="button" title="charles_wangw_1-1693478613716.png" alt="charles_wangw_1-1693478613716.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;charles_wangw_1-1693478613716.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;We think it should not stop while between the two sectors. And we compared to the version&amp;nbsp;&lt;SPAN&gt;&lt;SPAN class=""&gt;Fls_TS_T40D2M10I2R0. It works fine.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;Please help to check if there is some bugs in&amp;nbsp;Fls_TS_T40D2M10I1R0 for this part.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;Thanks&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;Charles&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 31 Aug 2023 10:48:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Write-fail-between-two-sectors-with-same-cluster/m-p/1714985#M26666</guid>
      <dc:creator>charles_wangw</dc:creator>
      <dc:date>2023-08-31T10:48:02Z</dc:date>
    </item>
    <item>
      <title>Re: Write fail between two sectors with same cluster</title>
      <link>https://community.nxp.com/t5/S32K/Write-fail-between-two-sectors-with-same-cluster/m-p/1739960#M27851</link>
      <description>&lt;P&gt;This thread is duplicated with below thread:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K/Fls-module-return-a-error-length-when-Fee-block-data-through-two/td-p/1713047" target="_blank"&gt;https://community.nxp.com/t5/S32K/Fls-module-return-a-error-length-when-Fee-block-data-through-two/td-p/1713047&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 16 Oct 2023 04:06:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Write-fail-between-two-sectors-with-same-cluster/m-p/1739960#M27851</guid>
      <dc:creator>cuongnguyenphu</dc:creator>
      <dc:date>2023-10-16T04:06:10Z</dc:date>
    </item>
  </channel>
</rss>