<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SHE-key attribute flags in S32K</title>
    <link>https://community.nxp.com/t5/S32K/SHE-key-attribute-flags/m-p/1735873#M27691</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm working in a project having the CSEc module (microcontroller S32K144). I know that, in order to update SHE-keys, 5 flags must be configured in order to generate the key in the M-format (Write Protection,&amp;nbsp;Boot Protection,&amp;nbsp;Debugger Usage Protection,&amp;nbsp;Wildcard Protection and&amp;nbsp;Key Usage Flag).&lt;/P&gt;&lt;P&gt;In some documents, I read also about Verify Only flag: if set when the key is used for CMAC, it can be used only to verify CMAC, otherwise the key can be used for verification and generation.&lt;/P&gt;&lt;P&gt;The question is: the flags are actually 5? what about the Verify Only flag?&lt;/P&gt;&lt;P&gt;Thank you in advance&lt;/P&gt;</description>
    <pubDate>Mon, 09 Oct 2023 15:11:39 GMT</pubDate>
    <dc:creator>ale_di_vi</dc:creator>
    <dc:date>2023-10-09T15:11:39Z</dc:date>
    <item>
      <title>SHE-key attribute flags</title>
      <link>https://community.nxp.com/t5/S32K/SHE-key-attribute-flags/m-p/1735873#M27691</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm working in a project having the CSEc module (microcontroller S32K144). I know that, in order to update SHE-keys, 5 flags must be configured in order to generate the key in the M-format (Write Protection,&amp;nbsp;Boot Protection,&amp;nbsp;Debugger Usage Protection,&amp;nbsp;Wildcard Protection and&amp;nbsp;Key Usage Flag).&lt;/P&gt;&lt;P&gt;In some documents, I read also about Verify Only flag: if set when the key is used for CMAC, it can be used only to verify CMAC, otherwise the key can be used for verification and generation.&lt;/P&gt;&lt;P&gt;The question is: the flags are actually 5? what about the Verify Only flag?&lt;/P&gt;&lt;P&gt;Thank you in advance&lt;/P&gt;</description>
      <pubDate>Mon, 09 Oct 2023 15:11:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SHE-key-attribute-flags/m-p/1735873#M27691</guid>
      <dc:creator>ale_di_vi</dc:creator>
      <dc:date>2023-10-09T15:11:39Z</dc:date>
    </item>
    <item>
      <title>Re: SHE-key attribute flags</title>
      <link>https://community.nxp.com/t5/S32K/SHE-key-attribute-flags/m-p/1736468#M27720</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/218511"&gt;@ale_di_vi&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;This is an extension to SHE specification. Search for "SFE" keyword (Security Flag Extension) in the reference manual and in the application note AN5401. This is a screenshot from the reference manual, description of Program Partition command:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lukaszadrapa_0-1696930974908.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/244267i9E3F075107FC2A63/image-size/medium?v=v2&amp;amp;px=400" role="button" title="lukaszadrapa_0-1696930974908.png" alt="lukaszadrapa_0-1696930974908.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;lukaszadrapa_0-1696930974908.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you don't want to use this extension, just keep SFE as 0 when running Program Partition command.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Tue, 10 Oct 2023 09:45:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SHE-key-attribute-flags/m-p/1736468#M27720</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2023-10-10T09:45:16Z</dc:date>
    </item>
    <item>
      <title>Re: SHE-key attribute flags</title>
      <link>https://community.nxp.com/t5/S32K/SHE-key-attribute-flags/m-p/1740507#M27876</link>
      <description>Ok, now it is clear.&lt;BR /&gt;Many thanks!</description>
      <pubDate>Mon, 16 Oct 2023 14:48:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SHE-key-attribute-flags/m-p/1740507#M27876</guid>
      <dc:creator>ale_di_vi</dc:creator>
      <dc:date>2023-10-16T14:48:46Z</dc:date>
    </item>
  </channel>
</rss>