<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: MCSPTEAK116 Motor Overcurrent continuous Fault</title>
    <link>https://community.nxp.com/t5/S32K/MCSPTEAK116-Motor-Overcurrent-continuous-Fault/m-p/1734943#M27608</link>
    <description>&lt;P&gt;I was missing J15. After inserting it, I could at least start the motor.&lt;/P&gt;&lt;P&gt;That leads me to a new problem, though I will start a different thread for that.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 06 Oct 2023 15:35:46 GMT</pubDate>
    <dc:creator>hns80</dc:creator>
    <dc:date>2023-10-06T15:35:46Z</dc:date>
    <item>
      <title>MCSPTEAK116 Motor Overcurrent continuous Fault</title>
      <link>https://community.nxp.com/t5/S32K/MCSPTEAK116-Motor-Overcurrent-continuous-Fault/m-p/1732785#M27516</link>
      <description>&lt;P&gt;I am trying to run the MCSPTE1AK116_PMSM_FOC_1Sh example on the S32K116 EVK and MOTOR-GD daughterboard. I was able to build the code and run it on the micro through the debugger.&lt;/P&gt;&lt;P&gt;When I run FreeMaster, the OverPhaseACurrent fault gets set immediately. This occurs even if I disconnect the motor completely from the board.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="hns80_0-1696281453533.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/243413iA8C9A201F8F4DE73/image-size/medium?v=v2&amp;amp;px=400" role="button" title="hns80_0-1696281453533.png" alt="hns80_0-1696281453533.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;hns80_0-1696281453533.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;When I stop FreeMaster and enter the debugger, I see this fault getting set.&lt;/P&gt;&lt;P&gt;Is there some setting that needs to change before building the code?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 02 Oct 2023 21:24:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MCSPTEAK116-Motor-Overcurrent-continuous-Fault/m-p/1732785#M27516</guid>
      <dc:creator>hns80</dc:creator>
      <dc:date>2023-10-02T21:24:25Z</dc:date>
    </item>
    <item>
      <title>Re: MCSPTEAK116 Motor Overcurrent continuous Fault</title>
      <link>https://community.nxp.com/t5/S32K/MCSPTEAK116-Motor-Overcurrent-continuous-Fault/m-p/1733170#M27535</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;have you set boards jumper properly on boards and also set overcurrent potentiometer as Get started guide mentions?&lt;BR /&gt;&lt;A href="https://www.nxp.com/document/guide/get-started-with-the-mcspte1ak116:GS-MCSPTE1AK116?section=plug-it-in" target="_blank"&gt;https://www.nxp.com/document/guide/get-started-with-the-mcspte1ak116:GS-MCSPTE1AK116?section=plug-it-in&lt;/A&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Tue, 03 Oct 2023 13:40:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MCSPTEAK116-Motor-Overcurrent-continuous-Fault/m-p/1733170#M27535</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-10-03T13:40:33Z</dc:date>
    </item>
    <item>
      <title>Re: MCSPTEAK116 Motor Overcurrent continuous Fault</title>
      <link>https://community.nxp.com/t5/S32K/MCSPTEAK116-Motor-Overcurrent-continuous-Fault/m-p/1734943#M27608</link>
      <description>&lt;P&gt;I was missing J15. After inserting it, I could at least start the motor.&lt;/P&gt;&lt;P&gt;That leads me to a new problem, though I will start a different thread for that.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 06 Oct 2023 15:35:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MCSPTEAK116-Motor-Overcurrent-continuous-Fault/m-p/1734943#M27608</guid>
      <dc:creator>hns80</dc:creator>
      <dc:date>2023-10-06T15:35:46Z</dc:date>
    </item>
  </channel>
</rss>