<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K144 P_FLASH in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-P-FLASH/m-p/802252#M2753</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I assume that the interrupt vector table and the timer interrupt handler are located in PFlash.&lt;/P&gt;&lt;P&gt;The S32K144 MCU has only one PFlash block&amp;nbsp;that can't be programmed and read&amp;nbsp;simultaneously.&lt;/P&gt;&lt;P&gt;See&amp;nbsp;36.5.9.4 Allowed simultaneous flash operations, S32K1xx RM, rev.9.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 16 Dec 2018 17:50:34 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2018-12-16T17:50:34Z</dc:date>
    <item>
      <title>S32K144 P_FLASH</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-P-FLASH/m-p/802251#M2752</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;Now I am writing the funciton of erase p_flash .My method is that follow that.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/69844i7EC050B547E40DDA/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;when I disable the timer interrupt,the p_flash 0x19000 can be written. But when I open the timer interrupt ,the mcu would reset. So,When I write p_flash,the interrupt should be colased?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 16 Dec 2018 03:11:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-P-FLASH/m-p/802251#M2752</guid>
      <dc:creator>玉敏111田</dc:creator>
      <dc:date>2018-12-16T03:11:19Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 P_FLASH</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-P-FLASH/m-p/802252#M2753</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I assume that the interrupt vector table and the timer interrupt handler are located in PFlash.&lt;/P&gt;&lt;P&gt;The S32K144 MCU has only one PFlash block&amp;nbsp;that can't be programmed and read&amp;nbsp;simultaneously.&lt;/P&gt;&lt;P&gt;See&amp;nbsp;36.5.9.4 Allowed simultaneous flash operations, S32K1xx RM, rev.9.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 16 Dec 2018 17:50:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-P-FLASH/m-p/802252#M2753</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-12-16T17:50:34Z</dc:date>
    </item>
  </channel>
</rss>