<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: s32k144 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/s32k144/m-p/1731832#M27480</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205585"&gt;@zhouqicheng&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;this is very general description. There could be a lot of reasons for this. First step is to attach a debugger and check if the bootloader is still in place and then check where the code is hanging or what actually happened. Without this, I'm not able to help.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
    <pubDate>Fri, 29 Sep 2023 07:09:08 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2023-09-29T07:09:08Z</dc:date>
    <item>
      <title>s32k144</title>
      <link>https://community.nxp.com/t5/S32K/s32k144/m-p/1730023#M27407</link>
      <description>&lt;P&gt;Hello, bootlaoder communication burning. After modifying the hardware, I found that when burning the program, sometimes I found that all can messages were 0 and could not be burned. I asked if it was possible that there was a problem with the can chip or that the mcu BootLoader area was damaged, and what could be the reason for this&lt;/P&gt;</description>
      <pubDate>Wed, 27 Sep 2023 01:58:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144/m-p/1730023#M27407</guid>
      <dc:creator>zhouqicheng</dc:creator>
      <dc:date>2023-09-27T01:58:09Z</dc:date>
    </item>
    <item>
      <title>Re: s32k144</title>
      <link>https://community.nxp.com/t5/S32K/s32k144/m-p/1731832#M27480</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205585"&gt;@zhouqicheng&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;this is very general description. There could be a lot of reasons for this. First step is to attach a debugger and check if the bootloader is still in place and then check where the code is hanging or what actually happened. Without this, I'm not able to help.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Fri, 29 Sep 2023 07:09:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144/m-p/1731832#M27480</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2023-09-29T07:09:08Z</dc:date>
    </item>
  </channel>
</rss>