<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K148EVB + ADTJA1101-RMII</title>
    <link>https://community.nxp.com/t5/S32K/S32K148EVB-ADTJA1101-RMII/m-p/802218#M2742</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have S32K148EVB-Q176 29643 REV C and ADTJA1101-RMII 30211 REV B. I would like to run lwIP TCP/IP stack demo application from S32 SDK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Should lwip_s32k148 from S32K14x EAR SDK v0.8.6 Example Project run on my unmodified S32K148EVB-Q176?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Demo app description says:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; In order for the example to work, resistors R123 and R514 must be populated and resistors R137 and R96 depopulated.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; These changes are in place on the S32K148 EVB (RevC).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have RevC board but the R137 is populated and R123 is depopulated. Should I unsolder resistor from R137 and solder in R123?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, is the demo app suppose to work without any modifications as the demo description suggests? Or should I add the proper PHY driver for TJA1101 in Processor Expert and then add some function calls in enetif_low_level_init to initialize PHY?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Marcin Miklas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Oct 2018 11:29:24 GMT</pubDate>
    <dc:creator>marcinmiklas</dc:creator>
    <dc:date>2018-10-17T11:29:24Z</dc:date>
    <item>
      <title>S32K148EVB + ADTJA1101-RMII</title>
      <link>https://community.nxp.com/t5/S32K/S32K148EVB-ADTJA1101-RMII/m-p/802218#M2742</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have S32K148EVB-Q176 29643 REV C and ADTJA1101-RMII 30211 REV B. I would like to run lwIP TCP/IP stack demo application from S32 SDK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Should lwip_s32k148 from S32K14x EAR SDK v0.8.6 Example Project run on my unmodified S32K148EVB-Q176?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Demo app description says:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; In order for the example to work, resistors R123 and R514 must be populated and resistors R137 and R96 depopulated.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; These changes are in place on the S32K148 EVB (RevC).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have RevC board but the R137 is populated and R123 is depopulated. Should I unsolder resistor from R137 and solder in R123?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, is the demo app suppose to work without any modifications as the demo description suggests? Or should I add the proper PHY driver for TJA1101 in Processor Expert and then add some function calls in enetif_low_level_init to initialize PHY?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Marcin Miklas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Oct 2018 11:29:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148EVB-ADTJA1101-RMII/m-p/802218#M2742</guid>
      <dc:creator>marcinmiklas</dc:creator>
      <dc:date>2018-10-17T11:29:24Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148EVB + ADTJA1101-RMII</title>
      <link>https://community.nxp.com/t5/S32K/S32K148EVB-ADTJA1101-RMII/m-p/802219#M2743</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Marcin,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Looks like there is a mistake in the example documentation, the resistors are OK in your configuration. &lt;SPAN&gt;S32K148EVB-Q176 29643 REV C&amp;nbsp;&lt;/SPAN&gt;shouldn't need any reworks.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;There is no need to include the PHY driver in the example, it should work without any modification.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Are you experiencing any issues with running the example?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Veronica&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Oct 2018 11:51:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148EVB-ADTJA1101-RMII/m-p/802219#M2743</guid>
      <dc:creator>veronicavelciu</dc:creator>
      <dc:date>2018-10-18T11:51:43Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148EVB + ADTJA1101-RMII</title>
      <link>https://community.nxp.com/t5/S32K/S32K148EVB-ADTJA1101-RMII/m-p/802220#M2744</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I run the example is enetif_low_level_output() is called 4 times with success and fifth time it gets stack there and never returns. It is because ENET_TX_QUEUE_FULL.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Assuming that no software changes are required then maybe something wrong is with hardware?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here you can see my jumpers configuration, maybe you will notice something wrong.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="IMG_20181019_141104.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/75909iDE69EEC315B9A597/image-size/large?v=v2&amp;amp;px=999" role="button" title="IMG_20181019_141104.jpg" alt="IMG_20181019_141104.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also question is how should I configure my media converter to BR-Reach master or slave?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If this is know then the last thing to check is polarity of br-reach cable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am running example using Debug RAM PEmicro configuration from S32 Design Studio for ARM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Marcin Miklas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Oct 2018 13:00:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148EVB-ADTJA1101-RMII/m-p/802220#M2744</guid>
      <dc:creator>marcinmiklas</dc:creator>
      <dc:date>2018-10-19T13:00:44Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148EVB + ADTJA1101-RMII</title>
      <link>https://community.nxp.com/t5/S32K/S32K148EVB-ADTJA1101-RMII/m-p/802221#M2745</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see from the picture that you are powering the board through the microUSB connector. Could you also try to use 12V power supply and&amp;nbsp;the following jumper configuration for S32K148 EVB&amp;nbsp;(J18:1-2, J7:2-3, J8:1-2) and let me know the result?&lt;/P&gt;&lt;P&gt;According to the MAST/SLV jumper on the ADTJA1101-RMII, the adapter is configured as Slave, so the Media Converter should be configured as Master.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Veronica&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Oct 2018 14:16:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148EVB-ADTJA1101-RMII/m-p/802221#M2745</guid>
      <dc:creator>veronicavelciu</dc:creator>
      <dc:date>2018-10-22T14:16:41Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148EVB + ADTJA1101-RMII</title>
      <link>https://community.nxp.com/t5/S32K/S32K148EVB-ADTJA1101-RMII/m-p/802222#M2746</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Veronica, now with 12V power supply it just works. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does it mean that with just USB it won't work at all? Or some special jumper configuration is needed?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Oct 2018 10:08:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148EVB-ADTJA1101-RMII/m-p/802222#M2746</guid>
      <dc:creator>marcinmiklashar</dc:creator>
      <dc:date>2018-10-23T10:08:26Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148EVB + ADTJA1101-RMII</title>
      <link>https://community.nxp.com/t5/S32K/S32K148EVB-ADTJA1101-RMII/m-p/802223#M2747</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using the S32K148EVB-Q176 with the ADTJA1101-RMII. We were facing the same issue, now resolved with the 12V power supply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We noticed that the TJA1101 is working only when VDD is 5V and not 3.3V. We cannot figure out why.&amp;nbsp;Is it possible to use it and run the demo using VDD 3.3V?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Feb 2019 13:46:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148EVB-ADTJA1101-RMII/m-p/802223#M2747</guid>
      <dc:creator>gabriel_robert</dc:creator>
      <dc:date>2019-02-27T13:46:44Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148EVB + ADTJA1101-RMII</title>
      <link>https://community.nxp.com/t5/S32K/S32K148EVB-ADTJA1101-RMII/m-p/802224#M2748</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Gabriel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is possible to run using VDD 3.3V by adding the following code to your demo:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;uint16_t regVal;&lt;BR /&gt; ENET_DRV_MDIORead(ENET_INSTANCE, 0, 17, &amp;amp;regVal, 65536);&lt;BR /&gt; regVal |= 0x4;&lt;BR /&gt; ENET_DRV_MDIOWrite(ENET_INSTANCE, 0, 17, regVal, 65536);&lt;/P&gt;&lt;P&gt;regVal = 0;&lt;BR /&gt; ENET_DRV_MDIORead(ENET_INSTANCE, 0, 18, &amp;amp;regVal, 65536);&lt;BR /&gt; ENET_DRV_MDIOWrite(ENET_INSTANCE, 0, 18, 0x5A11, 65536);&lt;BR /&gt; regVal = 0;&lt;BR /&gt; ENET_DRV_MDIORead(ENET_INSTANCE, 0, 18, &amp;amp;regVal, 65536);&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;This code makes the following transceiver configurations:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;PHY configured as Slave (if you want to configure as Master, use 0xDA11 instead of 0x5A11)&lt;/LI&gt;&lt;LI&gt;RMII mode enabled (50 MHz output on REF_CLK)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Please note that this code should be added after enabling the MDIO interface (using &lt;EM&gt;ENET_DRV_EnableMDIO&lt;/EM&gt;) and before any transmission/reception.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Veronica&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Mar 2019 15:56:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148EVB-ADTJA1101-RMII/m-p/802224#M2748</guid>
      <dc:creator>veronicavelciu</dc:creator>
      <dc:date>2019-03-11T15:56:48Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148EVB + ADTJA1101-RMII</title>
      <link>https://community.nxp.com/t5/S32K/S32K148EVB-ADTJA1101-RMII/m-p/802225#M2749</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does it works with the lwip sample? In that case, I have to add the enet module, but&amp;nbsp;the sample doesn't&amp;nbsp;work anymore if I just call&amp;nbsp;ENET_DRV_EnableMDIO ( in 5V or 3.3V ), or&amp;nbsp;ENET_DRV_EnableMDIO, and&amp;nbsp;then set the register you mentioned.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Gabriel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Mar 2019 16:44:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148EVB-ADTJA1101-RMII/m-p/802225#M2749</guid>
      <dc:creator>gabriel_robert</dc:creator>
      <dc:date>2019-03-11T16:44:09Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148EVB + ADTJA1101-RMII</title>
      <link>https://community.nxp.com/t5/S32K/S32K148EVB-ADTJA1101-RMII/m-p/802226#M2750</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Gabriel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The &lt;EM&gt;lwip&lt;/EM&gt; example already uses the ENET driver, initializes it and enables the MDIO interface. This is done in the&amp;nbsp;&lt;EM&gt;middleware\tcpip\tcpip_stack\ports\netif\enetif\enetif.c&lt;/EM&gt; file. You could add the code I mentioned after the following line:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;ENET_DRV_EnableMDIO(ENET_INSTANCE, false);&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know if this works for you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Veronica&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Mar 2019 06:41:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148EVB-ADTJA1101-RMII/m-p/802226#M2750</guid>
      <dc:creator>veronicavelciu</dc:creator>
      <dc:date>2019-03-12T06:41:02Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148EVB + ADTJA1101-RMII</title>
      <link>https://community.nxp.com/t5/S32K/S32K148EVB-ADTJA1101-RMII/m-p/802227#M2751</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot, it works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Mar 2019 08:55:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148EVB-ADTJA1101-RMII/m-p/802227#M2751</guid>
      <dc:creator>gabriel_robert</dc:creator>
      <dc:date>2019-03-12T08:55:21Z</dc:date>
    </item>
  </channel>
</rss>