<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: CAN_PAL returns STATUS_BUSY</title>
    <link>https://community.nxp.com/t5/S32K/CAN-PAL-returns-STATUS-BUSY/m-p/1727186#M27289</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;what is the board you are using? Do you have CAN transceiver active? What is the other node connected to your CAN bus? Do you see any signal on CAN lines? Does the module detect any kind of error (see ECR, ESR1 registers)?&lt;BR /&gt;There is can_pal demo example within SDK installation so you can refer to it.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Thu, 21 Sep 2023 13:43:37 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2023-09-21T13:43:37Z</dc:date>
    <item>
      <title>CAN_PAL returns STATUS_BUSY</title>
      <link>https://community.nxp.com/t5/S32K/CAN-PAL-returns-STATUS-BUSY/m-p/1727136#M27285</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have successfully initialized CAN with 500kbps and&amp;nbsp;CAN_ConfigTxBuff using CAN_PAL and when i tried to send a message using CAN_SEND its not working, while debugging got to know&amp;nbsp;FLEXCAN_StartSendData returning STATUS_BUSY and exiting. why its happening and how to rectify this problem?&lt;/P&gt;</description>
      <pubDate>Thu, 21 Sep 2023 12:11:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-PAL-returns-STATUS-BUSY/m-p/1727136#M27285</guid>
      <dc:creator>samvidh</dc:creator>
      <dc:date>2023-09-21T12:11:11Z</dc:date>
    </item>
    <item>
      <title>Re: CAN_PAL returns STATUS_BUSY</title>
      <link>https://community.nxp.com/t5/S32K/CAN-PAL-returns-STATUS-BUSY/m-p/1727186#M27289</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;what is the board you are using? Do you have CAN transceiver active? What is the other node connected to your CAN bus? Do you see any signal on CAN lines? Does the module detect any kind of error (see ECR, ESR1 registers)?&lt;BR /&gt;There is can_pal demo example within SDK installation so you can refer to it.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Thu, 21 Sep 2023 13:43:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-PAL-returns-STATUS-BUSY/m-p/1727186#M27289</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-09-21T13:43:37Z</dc:date>
    </item>
    <item>
      <title>Re: CAN_PAL returns STATUS_BUSY</title>
      <link>https://community.nxp.com/t5/S32K/CAN-PAL-returns-STATUS-BUSY/m-p/1727364#M27292</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using s32k144 microcontroller with custom board, have an can transceiver and using bus master to check for CAN messages on the bus, and can see only a error message on the bus and not sure About ECR and ESR1 registers.&lt;/P&gt;&lt;P&gt;Hope this helps you to answer!!&lt;/P&gt;</description>
      <pubDate>Fri, 22 Sep 2023 06:09:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-PAL-returns-STATUS-BUSY/m-p/1727364#M27292</guid>
      <dc:creator>samvidh</dc:creator>
      <dc:date>2023-09-22T06:09:44Z</dc:date>
    </item>
    <item>
      <title>Re: CAN_PAL returns STATUS_BUSY</title>
      <link>https://community.nxp.com/t5/S32K/CAN-PAL-returns-STATUS-BUSY/m-p/1727801#M27312</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;FlexCAN's&amp;nbsp;&lt;SPAN&gt;ECR and ESR1 registers can give you info about type of error detected by FlexCAN module.&lt;BR /&gt;Check it within debugger or read within code. If you see message transmitted by your MCU on the&amp;nbsp;bus, but terminated by error frame, it could be simply wrong CAN bit timing setting, be sure it is set similarly for each node connected.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 22 Sep 2023 07:48:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-PAL-returns-STATUS-BUSY/m-p/1727801#M27312</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-09-22T07:48:11Z</dc:date>
    </item>
    <item>
      <title>Re: CAN_PAL returns STATUS_BUSY</title>
      <link>https://community.nxp.com/t5/S32K/CAN-PAL-returns-STATUS-BUSY/m-p/1732295#M27492</link>
      <description>&lt;P&gt;its working now thankyou..&lt;/P&gt;</description>
      <pubDate>Sat, 30 Sep 2023 09:19:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-PAL-returns-STATUS-BUSY/m-p/1732295#M27492</guid>
      <dc:creator>samvidh</dc:creator>
      <dc:date>2023-09-30T09:19:48Z</dc:date>
    </item>
  </channel>
</rss>