<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: How to send a CAN message only 1 time</title>
    <link>https://community.nxp.com/t5/S32K/How-to-send-a-CAN-message-only-1-time/m-p/627267#M272</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;I connected PCB to VN1630.&lt;/P&gt;&lt;P&gt;Now I solved this problem. I changed CANsend code&amp;nbsp;from for(;;) to&amp;nbsp;LPIT ISR() and above situation was dissappeared.&lt;/P&gt;&lt;P&gt;I thought when I push the button CANsend code was activated several times.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Mar 2017 11:56:49 GMT</pubDate>
    <dc:creator>kimjunghyun</dc:creator>
    <dc:date>2017-03-09T11:56:49Z</dc:date>
    <item>
      <title>How to send a CAN message only 1 time</title>
      <link>https://community.nxp.com/t5/S32K/How-to-send-a-CAN-message-only-1-time/m-p/627265#M270</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;I try to send a CAN message and it works.&lt;/P&gt;&lt;P&gt;But there is a problem.&lt;/P&gt;&lt;P&gt;I send a CAN message only 1 time but several CAN messages are sent. (refer to below picture)&lt;/P&gt;&lt;P&gt;I have to send a CAN message only 1 time.&lt;/P&gt;&lt;P&gt;What should I do?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;■ MCU : S32K144(68pin)&lt;/P&gt;&lt;P&gt;■ Picture&lt;/P&gt;&lt;P&gt;&amp;nbsp; - 1 : CAN high at CAN transceiver&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;- 2 : CAN TX at MCU&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="scope_1.bmp"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/16508iEED3B35B8F04C888/image-size/large?v=v2&amp;amp;px=999" role="button" title="scope_1.bmp" alt="scope_1.bmp" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;■ Code&lt;/P&gt;&lt;P&gt;/* Including needed modules to compile this module/procedure */&lt;BR /&gt;#include "Cpu.h"&lt;BR /&gt;#include "pin_mux.h"&lt;BR /&gt;#include "clockMan1.h"&lt;BR /&gt;#include "dmaController1.h"&lt;BR /&gt;#include "osif1.h"&lt;BR /&gt;#include "canCom1.h"&lt;/P&gt;&lt;P&gt;&amp;nbsp; volatile int exit_code = 0;&lt;BR /&gt;/* User includes (#include below this line is not maintained by Processor Expert) */&lt;BR /&gt;&lt;STRONG&gt;#define MB (0UL)&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;#define MSG_ID 0x1B0 &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;/*!&lt;BR /&gt;&amp;nbsp; \brief The main function for the project.&lt;BR /&gt;&amp;nbsp; \details The startup initialization sequence is the following:&lt;BR /&gt;&amp;nbsp;* - startup asm routine&lt;BR /&gt;&amp;nbsp;* - main()&lt;BR /&gt;*/&lt;BR /&gt;int main(void)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp; /* Write your local variable definition here */&lt;BR /&gt;&amp;nbsp;&lt;STRONG&gt;flexcan_data_info_t dataInfo =&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;{&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;.data_length = 1U,&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;.msg_id_type = FLEXCAN_MSG_ID_STD,&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;.enable_brs = false,&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;.fd_enable = false,&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;.fd_padding = 0U&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;};&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;uint8_t toggleLED = 0x55;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; /*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/&lt;BR /&gt;&amp;nbsp; #ifdef PEX_RTOS_INIT&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PEX_RTOS_INIT();&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Initialization of the selected RTOS. Macro is defined by the RTOS component. */&lt;BR /&gt;&amp;nbsp; #endif&lt;BR /&gt;&amp;nbsp; /*** End of Processor Expert internal initialization.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ***/&lt;/P&gt;&lt;P&gt;&amp;nbsp; /* Write your code here */&lt;BR /&gt;&amp;nbsp; /* For example: for(;;) { } */&lt;BR /&gt;CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT, g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);&lt;BR /&gt;CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_FORCIBLE);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;STRONG&gt;FLEXCAN_DRV_Init(INST_CANCOM1, &amp;amp;canCom1_State, &amp;amp;canCom1_InitConfig0);&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;FLEXCAN_DRV_ConfigTxMb(INST_CANCOM1, MB, &amp;amp;dataInfo, MSG_ID);&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;for(;;)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;if(GPIO_HAL_ReadPins(PTD)&amp;gt;&amp;gt;0==1)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;GPIO_HAL_ClearPins(PTC,1&amp;lt;&amp;lt;0);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;STRONG&gt;FLEXCAN_DRV_Send(INST_CANCOM1, MB, &amp;amp;dataInfo, MSG_ID, &amp;amp;toggleLED);&amp;nbsp;&amp;nbsp;&lt;/STRONG&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;}&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;else&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;GPIO_HAL_SetPins(PTC,1&amp;lt;&amp;lt;0);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;}&lt;BR /&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Mar 2017 09:21:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-send-a-CAN-message-only-1-time/m-p/627265#M270</guid>
      <dc:creator>kimjunghyun</dc:creator>
      <dc:date>2017-03-07T09:21:28Z</dc:date>
    </item>
    <item>
      <title>Re: How to send a CAN message only 1 time</title>
      <link>https://community.nxp.com/t5/S32K/How-to-send-a-CAN-message-only-1-time/m-p/627266#M271</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not S32K SDK expert, but it looks like you did not receive acknowledge from receiving frame, so your microcontroller repeat the transmission again and again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the connected on your CAN bus? Is there any other device or microcontroller?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Mar 2017 12:59:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-send-a-CAN-message-only-1-time/m-p/627266#M271</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2017-03-07T12:59:01Z</dc:date>
    </item>
    <item>
      <title>Re: How to send a CAN message only 1 time</title>
      <link>https://community.nxp.com/t5/S32K/How-to-send-a-CAN-message-only-1-time/m-p/627267#M272</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;I connected PCB to VN1630.&lt;/P&gt;&lt;P&gt;Now I solved this problem. I changed CANsend code&amp;nbsp;from for(;;) to&amp;nbsp;LPIT ISR() and above situation was dissappeared.&lt;/P&gt;&lt;P&gt;I thought when I push the button CANsend code was activated several times.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Mar 2017 11:56:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-send-a-CAN-message-only-1-time/m-p/627267#M272</guid>
      <dc:creator>kimjunghyun</dc:creator>
      <dc:date>2017-03-09T11:56:49Z</dc:date>
    </item>
  </channel>
</rss>