<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K344_CAN_App_RTD200 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K344-CAN-App-RTD200/m-p/1722572#M27061</link>
    <description>&lt;P&gt;I would like to modify and run S32K344_CAN_App_RTD200 while S32K344_CAN_bootlloader_RTD2d0 is running. I am curious where to add the algorithms I wrote for acceleration sensor measurement, temperature measurement, etc. in the void APP_Demo_MainFun(void) function of S32K344_CAN_App_RTD200.&lt;/P&gt;&lt;P&gt;Can I define and add the user_Fun() function in the code below?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="UnLEE_1-1694648854260.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/240908i93AAD2DDE1D066AF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="UnLEE_1-1694648854260.png" alt="UnLEE_1-1694648854260.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;UnLEE_1-1694648854260.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the user_Fun() execution time is about 150ms, will there be any problem in executing the entire S32K344_CAN_App_RTD200 program? Because, in the APP_Demo_MainFun() function, TP_MainFun(); UDS_MainFun(); This is because I did not accurately understand its function and could not check if there was a timing problem. Also, I would appreciate it if you could explain this.&lt;/P&gt;</description>
    <pubDate>Wed, 13 Sep 2023 23:47:53 GMT</pubDate>
    <dc:creator>UnLEE</dc:creator>
    <dc:date>2023-09-13T23:47:53Z</dc:date>
    <item>
      <title>S32K344_CAN_App_RTD200</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-CAN-App-RTD200/m-p/1722572#M27061</link>
      <description>&lt;P&gt;I would like to modify and run S32K344_CAN_App_RTD200 while S32K344_CAN_bootlloader_RTD2d0 is running. I am curious where to add the algorithms I wrote for acceleration sensor measurement, temperature measurement, etc. in the void APP_Demo_MainFun(void) function of S32K344_CAN_App_RTD200.&lt;/P&gt;&lt;P&gt;Can I define and add the user_Fun() function in the code below?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="UnLEE_1-1694648854260.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/240908i93AAD2DDE1D066AF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="UnLEE_1-1694648854260.png" alt="UnLEE_1-1694648854260.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;UnLEE_1-1694648854260.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the user_Fun() execution time is about 150ms, will there be any problem in executing the entire S32K344_CAN_App_RTD200 program? Because, in the APP_Demo_MainFun() function, TP_MainFun(); UDS_MainFun(); This is because I did not accurately understand its function and could not check if there was a timing problem. Also, I would appreciate it if you could explain this.&lt;/P&gt;</description>
      <pubDate>Wed, 13 Sep 2023 23:47:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-CAN-App-RTD200/m-p/1722572#M27061</guid>
      <dc:creator>UnLEE</dc:creator>
      <dc:date>2023-09-13T23:47:53Z</dc:date>
    </item>
  </channel>
</rss>