<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: FlexCAN Module won't exit low power mode.</title>
    <link>https://community.nxp.com/t5/S32K/FlexCAN-Module-won-t-exit-low-power-mode/m-p/1720515#M26952</link>
    <description>Thank you so much! It looks my issue was that I wasn't enabling the MUX_3_DC_0 divider. I didn't think I would have to enable it since I didn't want to divide the FIRC rate but now that I did it works.</description>
    <pubDate>Mon, 11 Sep 2023 16:18:57 GMT</pubDate>
    <dc:creator>dane_vs10</dc:creator>
    <dc:date>2023-09-11T16:18:57Z</dc:date>
    <item>
      <title>FlexCAN Module won't exit low power mode.</title>
      <link>https://community.nxp.com/t5/S32K/FlexCAN-Module-won-t-exit-low-power-mode/m-p/1719693#M26921</link>
      <description>&lt;P&gt;Hello, I am attempting to setup the FlexCAN_0 module on a S32K344 development board. I cannot get the CAN module to exit low power mode.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have setup the external CAN pins and started the peripheral clock (Using FIRC, confirmed that it and BLOCK65 are on via FIRC.Status_Register and MC_ME.PRTN1_COFB2_STAT respectively.)&lt;/P&gt;&lt;P&gt;Then I set FlexCAN_0 MCR.MDIS to 0 which should enable the CAN module and turn off the Low Power Mode Enable bit (MCR bit 20). But the bit is never cleared. Is there something else I need to do before enabling the CAN module?&lt;/P&gt;</description>
      <pubDate>Fri, 08 Sep 2023 17:20:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FlexCAN-Module-won-t-exit-low-power-mode/m-p/1719693#M26921</guid>
      <dc:creator>dane_vs10</dc:creator>
      <dc:date>2023-09-08T17:20:16Z</dc:date>
    </item>
    <item>
      <title>Re: FlexCAN Module won't exit low power mode.</title>
      <link>https://community.nxp.com/t5/S32K/FlexCAN-Module-won-t-exit-low-power-mode/m-p/1719962#M26932</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@dane_vs10" target="_blank"&gt;Hi@dane_vs10&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;here is my test process, you can see it works on myside.(after init clock, just enable flexcan mode)&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_1-1694402170595.png" style="width: 690px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/240307i36C32B90AC4AB9FC/image-dimensions/690x398?v=v2" width="690" height="398" role="button" title="Senlent_1-1694402170595.png" alt="Senlent_1-1694402170595.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Senlent_1-1694402170595.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I guess the root cause is that you are not setting the flexcan module clock correctly,please check the highlighted part registers.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_0-1694402056524.png" style="width: 618px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/240305i050C8923D7778D69/image-dimensions/618x286?v=v2" width="618" height="286" role="button" title="Senlent_0-1694402056524.png" alt="Senlent_0-1694402056524.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Senlent_0-1694402056524.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR!&lt;/P&gt;</description>
      <pubDate>Mon, 11 Sep 2023 03:20:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FlexCAN-Module-won-t-exit-low-power-mode/m-p/1719962#M26932</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2023-09-11T03:20:57Z</dc:date>
    </item>
    <item>
      <title>Re: FlexCAN Module won't exit low power mode.</title>
      <link>https://community.nxp.com/t5/S32K/FlexCAN-Module-won-t-exit-low-power-mode/m-p/1720515#M26952</link>
      <description>Thank you so much! It looks my issue was that I wasn't enabling the MUX_3_DC_0 divider. I didn't think I would have to enable it since I didn't want to divide the FIRC rate but now that I did it works.</description>
      <pubDate>Mon, 11 Sep 2023 16:18:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FlexCAN-Module-won-t-exit-low-power-mode/m-p/1720515#M26952</guid>
      <dc:creator>dane_vs10</dc:creator>
      <dc:date>2023-09-11T16:18:57Z</dc:date>
    </item>
  </channel>
</rss>