<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K344CAN in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K344CAN/m-p/1720048#M26934</link>
    <description>&lt;P&gt;Hi, I'm trying to do a development board evaluation of the S32K344, and when I try to run the CAN part of the demo program, I find that the demo doesn't run as expected. The program will run into a file named starup, and according to the information I've checked, most of them are caused by a certain interrupt not being enabled, but it's obvious that this reason doesn't apply to explain the improper running of the demo program.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 11 Sep 2023 06:38:55 GMT</pubDate>
    <dc:creator>ShawnHuang</dc:creator>
    <dc:date>2023-09-11T06:38:55Z</dc:date>
    <item>
      <title>S32K344CAN</title>
      <link>https://community.nxp.com/t5/S32K/S32K344CAN/m-p/1720048#M26934</link>
      <description>&lt;P&gt;Hi, I'm trying to do a development board evaluation of the S32K344, and when I try to run the CAN part of the demo program, I find that the demo doesn't run as expected. The program will run into a file named starup, and according to the information I've checked, most of them are caused by a certain interrupt not being enabled, but it's obvious that this reason doesn't apply to explain the improper running of the demo program.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 11 Sep 2023 06:38:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344CAN/m-p/1720048#M26934</guid>
      <dc:creator>ShawnHuang</dc:creator>
      <dc:date>2023-09-11T06:38:55Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344CAN</title>
      <link>https://community.nxp.com/t5/S32K/S32K344CAN/m-p/1720214#M26941</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@ShawnHuang" target="_blank"&gt;Hi@ShawnHuang&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Are you testing the demo "FlexCAN_Ip_Example_S32K344"?&lt;/P&gt;
&lt;P&gt;in this demo, the flexcan works on loop-back mode and will exit while loop.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_0-1694422177720.png" style="width: 524px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/240382iFED1F002ADC5E141/image-dimensions/524x275?v=v2" width="524" height="275" role="button" title="Senlent_0-1694422177720.png" alt="Senlent_0-1694422177720.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Senlent_0-1694422177720.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;for s32k3x4EVB-q257, you can refer to this post:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-test-S32DS3-4/ta-p/1536225" target="_self"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-test-S32DS3-4/ta-p/1536225&lt;/A&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 11 Sep 2023 08:52:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344CAN/m-p/1720214#M26941</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2023-09-11T08:52:11Z</dc:date>
    </item>
  </channel>
</rss>