<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックICU S32K116</title>
    <link>https://community.nxp.com/t5/S32K/ICU-S32K116/m-p/1718979#M26889</link>
    <description>&lt;P&gt;"Hello NXP,&lt;/P&gt;&lt;P&gt;I am currently working with the Input Capture Module (ICU). I have configured it in the time stamp mode with a rising edge interrupt. Additionally,&lt;/P&gt;&lt;P&gt;I have set up FTM0 Channel 6. FTM0 is operating at an 8MHz SIRC clock, and I have configured the ICU channel with a prescaler of 128, resulting in a tick time of 16 microseconds.&lt;/P&gt;&lt;P&gt;With this configuration, the ICU channel can measure time intervals ranging from 16 microseconds to 1048560 microseconds, which is equivalent to over 1 second.&lt;/P&gt;&lt;P&gt;It works well with higher frequencies and shorter periods, from 16 microseconds up to 70 milliseconds. However, beyond 70 milliseconds, I encountered an issue where the values obtained include additional pulse ticks, as listed below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Ahmed_Attia_0-1694108249603.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/240083i33C5EF78588CD7F3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Ahmed_Attia_0-1694108249603.png" alt="Ahmed_Attia_0-1694108249603.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For 77 milliseconds, I observed a pulse with 3 additional ticks, indicating an error.&lt;/P&gt;&lt;P&gt;For 500 milliseconds (half a second), I observed a pulse with 10 additional ticks, and so on. I am curious if there is a specific reason for this behavior when working with lower frequencies.&lt;/P&gt;&lt;P&gt;Please note that I am using an NXP S32K116 microcontroller and configuring ADC0 using the TRESOS tool with the SW32K1_RTD_4.4_1.0.1_HF01_D2209 package."&lt;/P&gt;</description>
    <pubDate>Thu, 07 Sep 2023 17:38:42 GMT</pubDate>
    <dc:creator>Ahmed_Attia</dc:creator>
    <dc:date>2023-09-07T17:38:42Z</dc:date>
    <item>
      <title>ICU S32K116</title>
      <link>https://community.nxp.com/t5/S32K/ICU-S32K116/m-p/1718979#M26889</link>
      <description>&lt;P&gt;"Hello NXP,&lt;/P&gt;&lt;P&gt;I am currently working with the Input Capture Module (ICU). I have configured it in the time stamp mode with a rising edge interrupt. Additionally,&lt;/P&gt;&lt;P&gt;I have set up FTM0 Channel 6. FTM0 is operating at an 8MHz SIRC clock, and I have configured the ICU channel with a prescaler of 128, resulting in a tick time of 16 microseconds.&lt;/P&gt;&lt;P&gt;With this configuration, the ICU channel can measure time intervals ranging from 16 microseconds to 1048560 microseconds, which is equivalent to over 1 second.&lt;/P&gt;&lt;P&gt;It works well with higher frequencies and shorter periods, from 16 microseconds up to 70 milliseconds. However, beyond 70 milliseconds, I encountered an issue where the values obtained include additional pulse ticks, as listed below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Ahmed_Attia_0-1694108249603.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/240083i33C5EF78588CD7F3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Ahmed_Attia_0-1694108249603.png" alt="Ahmed_Attia_0-1694108249603.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For 77 milliseconds, I observed a pulse with 3 additional ticks, indicating an error.&lt;/P&gt;&lt;P&gt;For 500 milliseconds (half a second), I observed a pulse with 10 additional ticks, and so on. I am curious if there is a specific reason for this behavior when working with lower frequencies.&lt;/P&gt;&lt;P&gt;Please note that I am using an NXP S32K116 microcontroller and configuring ADC0 using the TRESOS tool with the SW32K1_RTD_4.4_1.0.1_HF01_D2209 package."&lt;/P&gt;</description>
      <pubDate>Thu, 07 Sep 2023 17:38:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ICU-S32K116/m-p/1718979#M26889</guid>
      <dc:creator>Ahmed_Attia</dc:creator>
      <dc:date>2023-09-07T17:38:42Z</dc:date>
    </item>
  </channel>
</rss>