<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic McuPeripheralClockConfig has not enough children in S32K</title>
    <link>https://community.nxp.com/t5/S32K/McuPeripheralClockConfig-has-not-enough-children/m-p/1718794#M26877</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;We are trying to walk through the demo application that Tresos provided us by default called simple_demo_can_rte. When we were at the &lt;STRONG&gt;Update BSW and SWC description wizard&lt;/STRONG&gt; step we encountered an error called&amp;nbsp;McuPeripheralClockConfig has not enough children says "It has 34 child - allowed are 41 to 41 child. The children are ..."&lt;/P&gt;&lt;P&gt;Note: We selected our board which is s32k148_lqfp176 in the dropdown located in the Resource_TS_T40D2M10I2R0 (ResourceSubderivative).&lt;BR /&gt;&lt;BR /&gt;When we selected the demo's default resourceSubderivative (s32k146_lqfp100) no errors occurred.&lt;/P&gt;&lt;P&gt;But in the boards folder (of simple_demo_can_rte project) which is located inside the source folder there is a default folder named FRDMK144_Q100_SCOS. This board is member of s32k144 family right? I am confused that when I select the s32k144_lqfp100 the same error occurred but with different child numbers.&lt;/P&gt;&lt;P&gt;Do you have any suggestion regarding McuClockSettingConfig error. For instance, adding the missing children? (We don't know what to add for s32k148_lqfp176)&lt;/P&gt;</description>
    <pubDate>Thu, 07 Sep 2023 11:59:33 GMT</pubDate>
    <dc:creator>gediz</dc:creator>
    <dc:date>2023-09-07T11:59:33Z</dc:date>
    <item>
      <title>McuPeripheralClockConfig has not enough children</title>
      <link>https://community.nxp.com/t5/S32K/McuPeripheralClockConfig-has-not-enough-children/m-p/1718794#M26877</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;We are trying to walk through the demo application that Tresos provided us by default called simple_demo_can_rte. When we were at the &lt;STRONG&gt;Update BSW and SWC description wizard&lt;/STRONG&gt; step we encountered an error called&amp;nbsp;McuPeripheralClockConfig has not enough children says "It has 34 child - allowed are 41 to 41 child. The children are ..."&lt;/P&gt;&lt;P&gt;Note: We selected our board which is s32k148_lqfp176 in the dropdown located in the Resource_TS_T40D2M10I2R0 (ResourceSubderivative).&lt;BR /&gt;&lt;BR /&gt;When we selected the demo's default resourceSubderivative (s32k146_lqfp100) no errors occurred.&lt;/P&gt;&lt;P&gt;But in the boards folder (of simple_demo_can_rte project) which is located inside the source folder there is a default folder named FRDMK144_Q100_SCOS. This board is member of s32k144 family right? I am confused that when I select the s32k144_lqfp100 the same error occurred but with different child numbers.&lt;/P&gt;&lt;P&gt;Do you have any suggestion regarding McuClockSettingConfig error. For instance, adding the missing children? (We don't know what to add for s32k148_lqfp176)&lt;/P&gt;</description>
      <pubDate>Thu, 07 Sep 2023 11:59:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/McuPeripheralClockConfig-has-not-enough-children/m-p/1718794#M26877</guid>
      <dc:creator>gediz</dc:creator>
      <dc:date>2023-09-07T11:59:33Z</dc:date>
    </item>
    <item>
      <title>Re: McuPeripheralClockConfig has not enough children</title>
      <link>https://community.nxp.com/t5/S32K/McuPeripheralClockConfig-has-not-enough-children/m-p/1721871#M27024</link>
      <description>&lt;P&gt;Which SW version your're using, I see the spanshot is so weird, ANd how did you take this Simple_demo_can_rte?&lt;BR /&gt;&lt;BR /&gt;The missing children can be added by click on the Plus button and select missing peripheral clock:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="cuongnguyenphu_0-1694594749013.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/240772i10805FA27744CC7F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="cuongnguyenphu_0-1694594749013.png" alt="cuongnguyenphu_0-1694594749013.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Sep 2023 08:45:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/McuPeripheralClockConfig-has-not-enough-children/m-p/1721871#M27024</guid>
      <dc:creator>cuongnguyenphu</dc:creator>
      <dc:date>2023-09-13T08:45:59Z</dc:date>
    </item>
  </channel>
</rss>