<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Possibility to use SPI manual software chip select</title>
    <link>https://community.nxp.com/t5/S32K/Possibility-to-use-SPI-manual-software-chip-select/m-p/1714002#M26621</link>
    <description>&lt;P&gt;Okey thank you for your response&lt;/P&gt;</description>
    <pubDate>Wed, 30 Aug 2023 11:38:33 GMT</pubDate>
    <dc:creator>elb1</dc:creator>
    <dc:date>2023-08-30T11:38:33Z</dc:date>
    <item>
      <title>Possibility to use SPI manual software chip select</title>
      <link>https://community.nxp.com/t5/S32K/Possibility-to-use-SPI-manual-software-chip-select/m-p/1635296#M22189</link>
      <description>&lt;P&gt;I am trying to communicate with the TLE94103 component using SPI (LPSPI0), is it possible to use some pin that has the GPIO function to operate as a chip-select pin and use the other SPI pins (CLK, MOSI, and MISO) in their usual pins that have the functionalities for SPI?&amp;nbsp;&lt;/P&gt;&lt;P&gt;and if I want to send and receive I am gonna first set the chip select GPIO to low and then set it to high after sending/receiving&lt;/P&gt;&lt;P&gt;is this possible?&lt;/P&gt;</description>
      <pubDate>Tue, 18 Apr 2023 09:19:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Possibility-to-use-SPI-manual-software-chip-select/m-p/1635296#M22189</guid>
      <dc:creator>Othmane1</dc:creator>
      <dc:date>2023-04-18T09:19:15Z</dc:date>
    </item>
    <item>
      <title>Re: Possibility to use SPI manual software chip select</title>
      <link>https://community.nxp.com/t5/S32K/Possibility-to-use-SPI-manual-software-chip-select/m-p/1635412#M22200</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210634"&gt;@Othmane1&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;You did not specify the part number.&lt;/P&gt;
&lt;P&gt;But yes, this is possible.&lt;/P&gt;
&lt;P&gt;The CS selected in the LPSPI module does not have to be routed to a pin.&lt;/P&gt;
&lt;P&gt;A GPIO can be used instead, but it would be your responsibility to assert and deassert the GPIO.&lt;/P&gt;
&lt;P&gt;Why do you need that?&lt;/P&gt;
&lt;P&gt;The LPSPI module allows configuring the PCS delays, frame size etc, it also allows continuous transfers with the CS asserted over multiple frames.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 18 Apr 2023 11:50:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Possibility-to-use-SPI-manual-software-chip-select/m-p/1635412#M22200</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2023-04-18T11:50:48Z</dc:date>
    </item>
    <item>
      <title>Re: Possibility to use SPI manual software chip select</title>
      <link>https://community.nxp.com/t5/S32K/Possibility-to-use-SPI-manual-software-chip-select/m-p/1713873#M26609</link>
      <description>&lt;P&gt;Hello, I have the same question but for different microcontrolller, is this (use chip select as gpio) also possible for mpc5748g ?&lt;BR /&gt;thank you&lt;/P&gt;</description>
      <pubDate>Wed, 30 Aug 2023 08:33:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Possibility-to-use-SPI-manual-software-chip-select/m-p/1713873#M26609</guid>
      <dc:creator>elb1</dc:creator>
      <dc:date>2023-08-30T08:33:59Z</dc:date>
    </item>
    <item>
      <title>Re: Possibility to use SPI manual software chip select</title>
      <link>https://community.nxp.com/t5/S32K/Possibility-to-use-SPI-manual-software-chip-select/m-p/1713889#M26613</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/216072"&gt;@elb1&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Yes, this is the same, the CS of the SPI module does not have to be used, it can be controlled by a GPIO.&lt;/P&gt;
&lt;P&gt;If you have any questions on mpc5748g, please create a new thread in the MPC5xxx community:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/MPC5xxx/bd-p/mpc5xxx" target="_blank"&gt;https://community.nxp.com/t5/MPC5xxx/bd-p/mpc5xxx&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 30 Aug 2023 08:48:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Possibility-to-use-SPI-manual-software-chip-select/m-p/1713889#M26613</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2023-08-30T08:48:08Z</dc:date>
    </item>
    <item>
      <title>Re: Possibility to use SPI manual software chip select</title>
      <link>https://community.nxp.com/t5/S32K/Possibility-to-use-SPI-manual-software-chip-select/m-p/1714002#M26621</link>
      <description>&lt;P&gt;Okey thank you for your response&lt;/P&gt;</description>
      <pubDate>Wed, 30 Aug 2023 11:38:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Possibility-to-use-SPI-manual-software-chip-select/m-p/1714002#M26621</guid>
      <dc:creator>elb1</dc:creator>
      <dc:date>2023-08-30T11:38:33Z</dc:date>
    </item>
  </channel>
</rss>