<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 S32K148 CAN issues</title>
    <link>https://community.nxp.com/t5/S32K/S32K148-CAN-issues/m-p/795500#M2657</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello NXP，&lt;/P&gt;&lt;P&gt;I have two questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SendCANData(18,CanTxId0[CanTxBCM_7F2h],BCM_7F2h._c,CanTxDLC0[CanTxBCM_7F2h]); //Cycle time:0ms&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;SendCANData(18,CanTxId0[CanTxBCM_786h],BCM_786h._c,CanTxDLC0[CanTxBCM_786h]); //Cycle time:0ms&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;SendCANData(18,CanTxId0[CanTxBCM_6E6h],BCM_6E6h._c,CanTxDLC0[CanTxBCM_6E6h]); //Cycle time:0ms&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;SendCANData(18,CanTxId0[CanTxBCM_6E5h],BCM_6E5h._c,CanTxDLC0[CanTxBCM_6E5h]); //Cycle time:0ms&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;SendCANData(18,CanTxId0[CanTxBCM_6E4h],BCM_6E4h._c,CanTxDLC0[CanTxBCM_6E4h]); //Cycle time:0ms&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;SendCANData(18,CanTxId0[CanTxBCM_401h],BCM_401h._c,CanTxDLC0[CanTxBCM_401h]); //Cycle time:0ms&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;SendCANData(18,CanTxId0[CanTxBCM_3C3h],BCM_3C3h._c,CanTxDLC0[CanTxBCM_3C3h]); //Cycle time:0ms&lt;/P&gt;&lt;P&gt;The send cycle time is 5ms;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SendCANData function is this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void SendCANData(uint32_t mailbox, uint32_t messageId, uint8_t * data, uint32_t len)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; flexcan_data_info_t dataInfo =&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .data_length = len,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .msg_id_type = FLEXCAN_MSG_ID_STD,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .enable_brs&amp;nbsp; = false,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .fd_enable&amp;nbsp;&amp;nbsp; = false,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .fd_padding&amp;nbsp; = 0U&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; };&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; FLEXCAN_DRV_ConfigTxMb(INST_CANCOM1, mailbox, &amp;amp;dataInfo, messageId);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; FLEXCAN_DRV_Send(INST_CANCOM1, mailbox, &amp;amp;dataInfo, messageId, data);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;/*Wait the CAN MB transfer successfully */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;//&lt;EM&gt;while(FLEXCAN_DRV_GetTransferStatus(INST_CANCOM1, mailbox) == STATUS_BUSY);&lt;/EM&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;delay_Nop(1000);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;case1： when I use the delay_Nop(1000), The send cycle is successful and receive can message is ok.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; but when I use the "&lt;EM&gt;while(FLEXCAN_DRV_GetTransferStatus(INST_CANCOM1, mailbox) == STATUS_BUSY);”， Send cycle is successful，but&amp;nbsp; the MCU can't entry the RXFIFO interrupt function to receive CAN message, why??&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;case 2:&amp;nbsp; When I use the delay_Nop(1000), Disconnect or Short Connect CAN Wire，After recovering the CAN wire to normal，CAN send cycle message can't be send successfully.&amp;nbsp; I check the status is "STATUS_CAN_NO_TRANSFER_IN_PROGRESS". What can I do? Thanks&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Nov 2018 06:06:46 GMT</pubDate>
    <dc:creator>hewei03</dc:creator>
    <dc:date>2018-11-23T06:06:46Z</dc:date>
    <item>
      <title>S32K148 CAN issues</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-CAN-issues/m-p/795500#M2657</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello NXP，&lt;/P&gt;&lt;P&gt;I have two questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SendCANData(18,CanTxId0[CanTxBCM_7F2h],BCM_7F2h._c,CanTxDLC0[CanTxBCM_7F2h]); //Cycle time:0ms&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;SendCANData(18,CanTxId0[CanTxBCM_786h],BCM_786h._c,CanTxDLC0[CanTxBCM_786h]); //Cycle time:0ms&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;SendCANData(18,CanTxId0[CanTxBCM_6E6h],BCM_6E6h._c,CanTxDLC0[CanTxBCM_6E6h]); //Cycle time:0ms&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;SendCANData(18,CanTxId0[CanTxBCM_6E5h],BCM_6E5h._c,CanTxDLC0[CanTxBCM_6E5h]); //Cycle time:0ms&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;SendCANData(18,CanTxId0[CanTxBCM_6E4h],BCM_6E4h._c,CanTxDLC0[CanTxBCM_6E4h]); //Cycle time:0ms&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;SendCANData(18,CanTxId0[CanTxBCM_401h],BCM_401h._c,CanTxDLC0[CanTxBCM_401h]); //Cycle time:0ms&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;SendCANData(18,CanTxId0[CanTxBCM_3C3h],BCM_3C3h._c,CanTxDLC0[CanTxBCM_3C3h]); //Cycle time:0ms&lt;/P&gt;&lt;P&gt;The send cycle time is 5ms;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SendCANData function is this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void SendCANData(uint32_t mailbox, uint32_t messageId, uint8_t * data, uint32_t len)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; flexcan_data_info_t dataInfo =&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .data_length = len,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .msg_id_type = FLEXCAN_MSG_ID_STD,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .enable_brs&amp;nbsp; = false,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .fd_enable&amp;nbsp;&amp;nbsp; = false,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .fd_padding&amp;nbsp; = 0U&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; };&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; FLEXCAN_DRV_ConfigTxMb(INST_CANCOM1, mailbox, &amp;amp;dataInfo, messageId);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; FLEXCAN_DRV_Send(INST_CANCOM1, mailbox, &amp;amp;dataInfo, messageId, data);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;/*Wait the CAN MB transfer successfully */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;//&lt;EM&gt;while(FLEXCAN_DRV_GetTransferStatus(INST_CANCOM1, mailbox) == STATUS_BUSY);&lt;/EM&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;delay_Nop(1000);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;case1： when I use the delay_Nop(1000), The send cycle is successful and receive can message is ok.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; but when I use the "&lt;EM&gt;while(FLEXCAN_DRV_GetTransferStatus(INST_CANCOM1, mailbox) == STATUS_BUSY);”， Send cycle is successful，but&amp;nbsp; the MCU can't entry the RXFIFO interrupt function to receive CAN message, why??&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;case 2:&amp;nbsp; When I use the delay_Nop(1000), Disconnect or Short Connect CAN Wire，After recovering the CAN wire to normal，CAN send cycle message can't be send successfully.&amp;nbsp; I check the status is "STATUS_CAN_NO_TRANSFER_IN_PROGRESS". What can I do? Thanks&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Nov 2018 06:06:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-CAN-issues/m-p/795500#M2657</guid>
      <dc:creator>hewei03</dc:creator>
      <dc:date>2018-11-23T06:06:46Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148 CAN issues</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-CAN-issues/m-p/795501#M2658</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;First of all let's start with the beginig of the problem.&lt;/P&gt;&lt;P&gt;1 What SDK Version you used ?&lt;/P&gt;&lt;P&gt;2 What CPU\Board used ?&lt;/P&gt;&lt;P&gt;3 What you want to do exactly ?&lt;/P&gt;&lt;P&gt;4. What is the driver configuration structure ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Nov 2018 15:00:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-CAN-issues/m-p/795501#M2658</guid>
      <dc:creator>alexandrunan</dc:creator>
      <dc:date>2018-11-27T15:00:02Z</dc:date>
    </item>
  </channel>
</rss>