<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Flash layout when using a bootloader on the S32K144 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Flash-layout-when-using-a-bootloader-on-the-S32K144/m-p/795296#M2656</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Damien,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I’m not familiar with this bootloader, but in general, there is no reason&amp;nbsp;for the "hole" between&amp;nbsp;m_flash_config&amp;nbsp;and m_text section, as you can see by&amp;nbsp;default&amp;nbsp;there is no any "hole".&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MCU reads the configuration (security, backdoor key, protection, …) from the location 0x400-0x410 (flash configuration field) which is a part of the bootloader.&lt;/P&gt;&lt;P&gt;You are right, there is no need for the section in the application.&lt;/P&gt;&lt;P&gt;Please refer to&amp;nbsp;36.4.1 Flash configuration field description in the reference manual S32K1xx RM, rev.8. There you can find the details.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The m_interrupts section should be at the 0x00000000 address in the bootloader project. Because the m_interrupts contains&amp;nbsp;stack pointer and reset vector which is expected always at the address 0x0 and 0x4.(The first 8B)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The&amp;nbsp;m_interrupts section in the application project starts at the beginning of the sector (0x00001000 - AN12218, 0x00004000 - S32K144 CAN bootloader,....). The reason is that the smallest unit which can be erased is 1 sector (4 KB).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I hope it helps you.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Diana&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 14 Sep 2018 14:13:58 GMT</pubDate>
    <dc:creator>dianabatrlova</dc:creator>
    <dc:date>2018-09-14T14:13:58Z</dc:date>
    <item>
      <title>Flash layout when using a bootloader on the S32K144</title>
      <link>https://community.nxp.com/t5/S32K/Flash-layout-when-using-a-bootloader-on-the-S32K144/m-p/795295#M2655</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am currently designing a bootloader for the S32K144, and I have some questions about the flash layout when using the bootloader.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When compiling a normal application (i.e. single program, no bootloader), there is a section of flash for the interrupts, a section of flash for the Flash configuration and the remainder for the program itself.&amp;nbsp; That is:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-none line-numbers"&gt;&lt;CODE&gt;/* Specify the memory areas */
MEMORY
{
&amp;nbsp; /* Flash */
&amp;nbsp; m_interrupts&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (RX)&amp;nbsp; : ORIGIN = 0x00000000, LENGTH = 0x00000400
&amp;nbsp; m_flash_config&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (RX)&amp;nbsp; : ORIGIN = 0x00000400, LENGTH = 0x00000010
&amp;nbsp; m_text&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (RX)&amp;nbsp; : ORIGIN = 0x00000410, LENGTH = 0x0007FBF0

&amp;nbsp; /* SRAM_L */
&amp;nbsp; m_data&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (RW)&amp;nbsp; : ORIGIN = 0x1FFF8000, LENGTH = 0x00008000

&amp;nbsp; /* SRAM_U */
&amp;nbsp; m_data_2&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (RW)&amp;nbsp; : ORIGIN = 0x20000000, LENGTH = 0x00007000
}
&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, the bootloader in the S32K144 CAN bootloader has an additional "hole" in the flash map between where the m_flash_config ends and the text section begins. Is there a reason for this hole?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-none line-numbers"&gt;&lt;CODE&gt;/* Specify the memory areas */
MEMORY
{
&amp;nbsp; m_interrupts&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (RX)&amp;nbsp; : ORIGIN = 0x00000000, LENGTH = 0x00000400
&amp;nbsp; m_flash_config&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (RX)&amp;nbsp; : ORIGIN = 0x00000400, LENGTH = 0x00000010
&amp;nbsp; /** Note the hole here between 0x410 and 0x500 **/
&amp;nbsp; m_text&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (RX)&amp;nbsp; : ORIGIN = 0x00000500, LENGTH = 512K - 0x500
&amp;nbsp; m_data&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (RW)&amp;nbsp; : ORIGIN = 0x1FFF8000, LENGTH = 0x00007FFF
&amp;nbsp; m_data_2&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (RW)&amp;nbsp; : ORIGIN = 0x20000000, LENGTH = 0x00007000
}
&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Secondly, when looking at AN12218 ("Using the bootloader, S32K1xx Bootloader,Rev. 0,07/2018", p8 sec.3), there is an explicit location in the user application for storage of the flash_config space, even through (as I understand it), they are read and applied only on reset and thus it is the value at 0x0400 in flash that really matters.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;IMG alt="pastedImage_1.png" src="https://community.nxp.com/t5/image/serverpage/image-id/68128i9B156631E0F1E5FB/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;The S32K144 CAN bootloader application keeps the flash_config in the expected location, and there is no "hole" for it in the memory map:&lt;/P&gt;&lt;PRE class="language-none line-numbers"&gt;&lt;CODE&gt;/* Specify the memory areas */
MEMORY
{
&amp;nbsp; m_interrupts&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (RX)&amp;nbsp; : ORIGIN = 0x00004000, LENGTH = 0x00000400
&amp;nbsp; m_flash_config&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (RX)&amp;nbsp; : ORIGIN = 0x00000400, LENGTH = 0x00000010
&amp;nbsp; m_text&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (RX)&amp;nbsp; : ORIGIN = 0x00004400, LENGTH = 512K - 0x4400
&amp;nbsp; m_data&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (RW)&amp;nbsp; : ORIGIN = 0x1FFF8000, LENGTH = 0x00007FFF
&amp;nbsp; m_data_2&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (RW)&amp;nbsp; : ORIGIN = 0x20000000, LENGTH = 0x00007000
}
&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does there need to be a section in flash reserved for the flash_config, even when in the application?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My second question is with respect to the alignment of m_interrupts.&amp;nbsp;&amp;nbsp; Does this need to be aligned with anything specific (e.g. 512-byte/1024-byte boundaries, a 4k sector of flash, etc)?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Nov 2020 14:10:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Flash-layout-when-using-a-bootloader-on-the-S32K144/m-p/795295#M2655</guid>
      <dc:creator>damiendusha</dc:creator>
      <dc:date>2020-11-02T14:10:13Z</dc:date>
    </item>
    <item>
      <title>Re: Flash layout when using a bootloader on the S32K144</title>
      <link>https://community.nxp.com/t5/S32K/Flash-layout-when-using-a-bootloader-on-the-S32K144/m-p/795296#M2656</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Damien,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I’m not familiar with this bootloader, but in general, there is no reason&amp;nbsp;for the "hole" between&amp;nbsp;m_flash_config&amp;nbsp;and m_text section, as you can see by&amp;nbsp;default&amp;nbsp;there is no any "hole".&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MCU reads the configuration (security, backdoor key, protection, …) from the location 0x400-0x410 (flash configuration field) which is a part of the bootloader.&lt;/P&gt;&lt;P&gt;You are right, there is no need for the section in the application.&lt;/P&gt;&lt;P&gt;Please refer to&amp;nbsp;36.4.1 Flash configuration field description in the reference manual S32K1xx RM, rev.8. There you can find the details.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The m_interrupts section should be at the 0x00000000 address in the bootloader project. Because the m_interrupts contains&amp;nbsp;stack pointer and reset vector which is expected always at the address 0x0 and 0x4.(The first 8B)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The&amp;nbsp;m_interrupts section in the application project starts at the beginning of the sector (0x00001000 - AN12218, 0x00004000 - S32K144 CAN bootloader,....). The reason is that the smallest unit which can be erased is 1 sector (4 KB).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I hope it helps you.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Diana&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Sep 2018 14:13:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Flash-layout-when-using-a-bootloader-on-the-S32K144/m-p/795296#M2656</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2018-09-14T14:13:58Z</dc:date>
    </item>
  </channel>
</rss>