<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K118 PIN in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K118-PIN/m-p/1712369#M26514</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/198746"&gt;@wenfengyao&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;It should be in HIGH-Z and the pin should read 0V in this case unless there is the internal pull-up enabled - which would explain the 900mV at the anode.&lt;/P&gt;
&lt;P&gt;The pullup is enabled on PTC5 by default, for example.&lt;/P&gt;
&lt;P&gt;Which pin do you use?&lt;/P&gt;
&lt;P&gt;What is the usecase here?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 31 Aug 2023 07:16:50 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2023-08-31T07:16:50Z</dc:date>
    <item>
      <title>S32K118 PIN</title>
      <link>https://community.nxp.com/t5/S32K/S32K118-PIN/m-p/1712258#M26502</link>
      <description>&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;We need to input the external high-low level signal to the 18 pin of the MCU in series with a diode. At the beginning, the pin is in the default state without configuration, and only the external interrupt is used. In this case, the MCU pin detected at low level has a voltage of 800 or 900mV;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt; When this pin is configured to the input (floating) state, the detected MCU pin has a voltage of about 0V at low voltage. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;Our software colleagues believe that the external interrupt input and the configuration pin input (floating) should be in a high resistance state, but the measured results are not the same, may I ask the specific difference between the two internal circuits?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt; What causes the low level input to have a voltage difference?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;The part number is FS32K118LAT0MLFT&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 28 Aug 2023 09:22:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K118-PIN/m-p/1712258#M26502</guid>
      <dc:creator>wenfengyao</dc:creator>
      <dc:date>2023-08-28T09:22:02Z</dc:date>
    </item>
    <item>
      <title>Re: S32K118 PIN</title>
      <link>https://community.nxp.com/t5/S32K/S32K118-PIN/m-p/1712369#M26514</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/198746"&gt;@wenfengyao&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;It should be in HIGH-Z and the pin should read 0V in this case unless there is the internal pull-up enabled - which would explain the 900mV at the anode.&lt;/P&gt;
&lt;P&gt;The pullup is enabled on PTC5 by default, for example.&lt;/P&gt;
&lt;P&gt;Which pin do you use?&lt;/P&gt;
&lt;P&gt;What is the usecase here?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 31 Aug 2023 07:16:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K118-PIN/m-p/1712369#M26514</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2023-08-31T07:16:50Z</dc:date>
    </item>
    <item>
      <title>Re: S32K118 PIN</title>
      <link>https://community.nxp.com/t5/S32K/S32K118-PIN/m-p/1714571#M26639</link>
      <description>I just want to use PIN 18 PTC5 pin to do an interrupt input, so the default state of this pin is pull-up?</description>
      <pubDate>Thu, 31 Aug 2023 02:55:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K118-PIN/m-p/1714571#M26639</guid>
      <dc:creator>wenfengyao</dc:creator>
      <dc:date>2023-08-31T02:55:14Z</dc:date>
    </item>
    <item>
      <title>Re: S32K118 PIN</title>
      <link>https://community.nxp.com/t5/S32K/S32K118-PIN/m-p/1714773#M26652</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/198746"&gt;@wenfengyao&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;PTC5 has internal pullup enabled by default out of reset.&lt;/P&gt;
&lt;P&gt;Please refer to&lt;/P&gt;
&lt;P&gt;S32K118 IO_Signal_Description_Input_Multiplexing.xlsx&lt;/P&gt;
&lt;P&gt;IO SIgnal Table&lt;/P&gt;
&lt;P&gt;Column S&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Thu, 31 Aug 2023 07:28:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K118-PIN/m-p/1714773#M26652</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2023-08-31T07:28:44Z</dc:date>
    </item>
  </channel>
</rss>