<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: S32K116  FTM input capture</title>
    <link>https://community.nxp.com/t5/S32K/S32K116-FTM-input-capture/m-p/1710178#M26408</link>
    <description>&lt;P&gt;I use&amp;nbsp;&lt;EM&gt;47.7.3 Channel (n) Interrupt&lt;/EM&gt; ,and the CHF flag is set.&lt;/P&gt;&lt;P&gt;I've used &lt;SPAN&gt;&amp;nbsp;the examples in the S32K1 SDK&lt;/SPAN&gt;, the phenomenon is the same。&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 24 Aug 2023 00:28:02 GMT</pubDate>
    <dc:creator>hanchengyu11</dc:creator>
    <dc:date>2023-08-24T00:28:02Z</dc:date>
    <item>
      <title>S32K116  FTM input capture</title>
      <link>https://community.nxp.com/t5/S32K/S32K116-FTM-input-capture/m-p/1709559#M26359</link>
      <description>&lt;P&gt;I set FTM0_CH4 for input capture（Capture on Rising Edge Only）.After ftm initialization is complete, an interrupt occurs，But there is no input change on the FTM0_CH4 pin。（This pin has to do 5v pull-up）&lt;/P&gt;</description>
      <pubDate>Wed, 23 Aug 2023 05:16:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K116-FTM-input-capture/m-p/1709559#M26359</guid>
      <dc:creator>hanchengyu11</dc:creator>
      <dc:date>2023-08-23T05:16:04Z</dc:date>
    </item>
    <item>
      <title>Re: S32K116  FTM input capture</title>
      <link>https://community.nxp.com/t5/S32K/S32K116-FTM-input-capture/m-p/1709880#M26393</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Which interrupt occurs after ftm initialization is complete? Did you check the flags?&amp;nbsp;&lt;BR /&gt;&lt;EM&gt;47.7.1 Timer Overflow Interrupt&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;The timer overflow interrupt is generated when (TOIE = 1) and (TOF = 1).&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;47.7.3 Channel (n) Interrupt&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;The channel (n) interrupt is generated when (CHIE = 1) and (CHF = 1).&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;Are you testing the code of &lt;STRONG&gt;3.5. Single-edge capture mode&lt;/STRONG&gt; of &lt;A href="https://www.nxp.com/docs/en/application-note/AN5303.pdf" target="_self"&gt;AN5303&lt;/A&gt; &lt;A href="https://www.nxp.com/webapp/Download?colCode=AN5303SW&amp;amp;docLang=en" target="_self"&gt;AN5303SW&lt;/A&gt;? Or test the examples in the S32K1 SDK?&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 23 Aug 2023 11:43:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K116-FTM-input-capture/m-p/1709880#M26393</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-08-23T11:43:37Z</dc:date>
    </item>
    <item>
      <title>Re: S32K116  FTM input capture</title>
      <link>https://community.nxp.com/t5/S32K/S32K116-FTM-input-capture/m-p/1710178#M26408</link>
      <description>&lt;P&gt;I use&amp;nbsp;&lt;EM&gt;47.7.3 Channel (n) Interrupt&lt;/EM&gt; ,and the CHF flag is set.&lt;/P&gt;&lt;P&gt;I've used &lt;SPAN&gt;&amp;nbsp;the examples in the S32K1 SDK&lt;/SPAN&gt;, the phenomenon is the same。&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 24 Aug 2023 00:28:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K116-FTM-input-capture/m-p/1710178#M26408</guid>
      <dc:creator>hanchengyu11</dc:creator>
      <dc:date>2023-08-24T00:28:02Z</dc:date>
    </item>
  </channel>
</rss>