<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CAN-Rx interrupt is not working in S32K</title>
    <link>https://community.nxp.com/t5/S32K/CAN-Rx-interrupt-is-not-working/m-p/1709883#M26394</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;teh usage of Callback is shown e.g. in&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-test-S32DS3-4/ta-p/1536225" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-test-S32DS3-4/ta-p/1536225&lt;/A&gt;&lt;BR /&gt;But it does not use OS, but maybe it could be usefull as well.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Wed, 23 Aug 2023 11:46:20 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2023-08-23T11:46:20Z</dc:date>
    <item>
      <title>CAN-Rx interrupt is not working</title>
      <link>https://community.nxp.com/t5/S32K/CAN-Rx-interrupt-is-not-working/m-p/1709250#M26332</link>
      <description>&lt;P&gt;Hi NXP team,&lt;BR /&gt;&lt;BR /&gt;I tried to work on the CAN-Rx interrupt.&lt;BR /&gt;&lt;BR /&gt;I configured CAN-Rx interrupt and I used ETAS- OS for interrupt callback triggering.&lt;BR /&gt;&lt;BR /&gt;But If i enable the&amp;nbsp;CAN-Rx interrupt Can't able to access the&amp;nbsp;interrupt callback definition while compilation itself getting linker error.&lt;BR /&gt;&lt;BR /&gt;Can you please help how to proceed on this&amp;nbsp;CAN-Rx interrupt.&lt;/P&gt;</description>
      <pubDate>Tue, 22 Aug 2023 15:42:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-Rx-interrupt-is-not-working/m-p/1709250#M26332</guid>
      <dc:creator>Venu_M</dc:creator>
      <dc:date>2023-08-22T15:42:13Z</dc:date>
    </item>
    <item>
      <title>Re: CAN-Rx interrupt is not working</title>
      <link>https://community.nxp.com/t5/S32K/CAN-Rx-interrupt-is-not-working/m-p/1709779#M26387</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;please specify the part you are using, the S32DS and RTD versions.&amp;nbsp;&lt;BR /&gt;Also share error message you got.&lt;/P&gt;
&lt;P&gt;BR, Petr&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Aug 2023 09:38:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-Rx-interrupt-is-not-working/m-p/1709779#M26387</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-08-23T09:38:00Z</dc:date>
    </item>
    <item>
      <title>Re: CAN-Rx interrupt is not working</title>
      <link>https://community.nxp.com/t5/S32K/CAN-Rx-interrupt-is-not-working/m-p/1709792#M26388</link>
      <description>&lt;P&gt;&lt;SPAN&gt;&lt;BR /&gt;Hi Petr,&lt;BR /&gt;&lt;BR /&gt;1.S32K342 MC and RTD versions is 2.0.0.&lt;BR /&gt;Now I'm trying to integrate with OS Isr for CAN- Rx , which Function I need to use for interrupt callback.&lt;BR /&gt;&lt;BR /&gt;How to access the Rx interrupt .&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Aug 2023 09:46:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-Rx-interrupt-is-not-working/m-p/1709792#M26388</guid>
      <dc:creator>Venu_M</dc:creator>
      <dc:date>2023-08-23T09:46:04Z</dc:date>
    </item>
    <item>
      <title>Re: CAN-Rx interrupt is not working</title>
      <link>https://community.nxp.com/t5/S32K/CAN-Rx-interrupt-is-not-working/m-p/1709883#M26394</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;teh usage of Callback is shown e.g. in&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-test-S32DS3-4/ta-p/1536225" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-test-S32DS3-4/ta-p/1536225&lt;/A&gt;&lt;BR /&gt;But it does not use OS, but maybe it could be usefull as well.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Wed, 23 Aug 2023 11:46:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-Rx-interrupt-is-not-working/m-p/1709883#M26394</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-08-23T11:46:20Z</dc:date>
    </item>
  </channel>
</rss>