<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Interfacing a buzzer with s32k118 microcontroller and also changing its frequency</title>
    <link>https://community.nxp.com/t5/S32K/Interfacing-a-buzzer-with-s32k118-microcontroller-and-also/m-p/1709519#M26355</link>
    <description>and im using the j4 ptd15 pin for the sample code ftm_pwm_s32k118 with a frequency of 2000u ,3000u changed in flexTimer_pwm_1_PwmConfig please help</description>
    <pubDate>Wed, 23 Aug 2023 03:34:25 GMT</pubDate>
    <dc:creator>SteveSam</dc:creator>
    <dc:date>2023-08-23T03:34:25Z</dc:date>
    <item>
      <title>Interfacing a buzzer with s32k118 microcontroller and also changing its frequency</title>
      <link>https://community.nxp.com/t5/S32K/Interfacing-a-buzzer-with-s32k118-microcontroller-and-also/m-p/1708136#M26259</link>
      <description>&lt;P&gt;Hi, Im new to the embedded world and just getting started...and i would like to know how to interface an buzzer with this board&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Steve&lt;/P&gt;</description>
      <pubDate>Mon, 21 Aug 2023 07:35:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Interfacing-a-buzzer-with-s32k118-microcontroller-and-also/m-p/1708136#M26259</guid>
      <dc:creator>SteveSam</dc:creator>
      <dc:date>2023-08-21T07:35:30Z</dc:date>
    </item>
    <item>
      <title>Re: Interfacing a buzzer with s32k118 microcontroller and also changing its frequency</title>
      <link>https://community.nxp.com/t5/S32K/Interfacing-a-buzzer-with-s32k118-microcontroller-and-also/m-p/1708784#M26300</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;depending on type of buzzer a direct connection to MCU output is most probably not possible and simple transistor should be used, like below.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PetrS_0-1692685177024.png" style="width: 196px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/237363iABB4635E20CEEE81/image-dimensions/196x166?v=v2" width="196" height="166" role="button" title="PetrS_0-1692685177024.png" alt="PetrS_0-1692685177024.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;If you want to generate PWM signal then choose a pin ideally&amp;nbsp;&lt;SPAN&gt;with FTM functionality. FTM channel can be configured for various output modes with PWM as well. Refer to device RM for more info.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Basic FTM examples can be found within S32 Design Studio.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Tue, 22 Aug 2023 06:20:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Interfacing-a-buzzer-with-s32k118-microcontroller-and-also/m-p/1708784#M26300</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-08-22T06:20:39Z</dc:date>
    </item>
    <item>
      <title>Re: Interfacing a buzzer with s32k118 microcontroller and also changing its frequency</title>
      <link>https://community.nxp.com/t5/S32K/Interfacing-a-buzzer-with-s32k118-microcontroller-and-also/m-p/1709292#M26334</link>
      <description>hi, Ive learnt how to generate a pwm signal and change its frequency but the buzzer still does not work...I have a buzzer with 3 pins (vcc,gnd,io ) and i wonder if still have to use a transistor.</description>
      <pubDate>Tue, 22 Aug 2023 17:23:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Interfacing-a-buzzer-with-s32k118-microcontroller-and-also/m-p/1709292#M26334</guid>
      <dc:creator>SteveSam</dc:creator>
      <dc:date>2023-08-22T17:23:13Z</dc:date>
    </item>
    <item>
      <title>Re: Interfacing a buzzer with s32k118 microcontroller and also changing its frequency</title>
      <link>https://community.nxp.com/t5/S32K/Interfacing-a-buzzer-with-s32k118-microcontroller-and-also/m-p/1709519#M26355</link>
      <description>and im using the j4 ptd15 pin for the sample code ftm_pwm_s32k118 with a frequency of 2000u ,3000u changed in flexTimer_pwm_1_PwmConfig please help</description>
      <pubDate>Wed, 23 Aug 2023 03:34:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Interfacing-a-buzzer-with-s32k118-microcontroller-and-also/m-p/1709519#M26355</guid>
      <dc:creator>SteveSam</dc:creator>
      <dc:date>2023-08-23T03:34:25Z</dc:date>
    </item>
  </channel>
</rss>