<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K310  PNE debugger</title>
    <link>https://community.nxp.com/t5/S32K/S32K310-PNE-debugger/m-p/1708585#M26286</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a S32K31X_Q100 which the micro is actually s32k311_q100.&lt;/P&gt;&lt;P&gt;while I can generate the code via&amp;nbsp; the PIN CONFIGURATION&amp;nbsp; module successfully, something peculiar happens that&amp;nbsp; keeps me just dizzy. I use a MULTILINK UNIVERSAL DEBUUGER box and when i create a debug configuration, the very first time the debug tool works fine. however when&amp;nbsp; I add or remove pins in the pin configuration module while the generated code as far as number of pins is ok , as soon as I connect the debugger all this updated micro and constants are not updated and the debugger loads the old values before the update. actually it uses the the very first configuration values.&lt;/P&gt;&lt;P&gt;every time I generate I update&amp;nbsp; &amp;nbsp;and do clean and build again however when I switch to debugger , it loads the original values.&lt;/P&gt;&lt;P&gt;Please help,&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Koorosh Hajiani&lt;/P&gt;</description>
    <pubDate>Mon, 21 Aug 2023 21:20:29 GMT</pubDate>
    <dc:creator>hajianik</dc:creator>
    <dc:date>2023-08-21T21:20:29Z</dc:date>
    <item>
      <title>S32K310  PNE debugger</title>
      <link>https://community.nxp.com/t5/S32K/S32K310-PNE-debugger/m-p/1708585#M26286</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a S32K31X_Q100 which the micro is actually s32k311_q100.&lt;/P&gt;&lt;P&gt;while I can generate the code via&amp;nbsp; the PIN CONFIGURATION&amp;nbsp; module successfully, something peculiar happens that&amp;nbsp; keeps me just dizzy. I use a MULTILINK UNIVERSAL DEBUUGER box and when i create a debug configuration, the very first time the debug tool works fine. however when&amp;nbsp; I add or remove pins in the pin configuration module while the generated code as far as number of pins is ok , as soon as I connect the debugger all this updated micro and constants are not updated and the debugger loads the old values before the update. actually it uses the the very first configuration values.&lt;/P&gt;&lt;P&gt;every time I generate I update&amp;nbsp; &amp;nbsp;and do clean and build again however when I switch to debugger , it loads the original values.&lt;/P&gt;&lt;P&gt;Please help,&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Koorosh Hajiani&lt;/P&gt;</description>
      <pubDate>Mon, 21 Aug 2023 21:20:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K310-PNE-debugger/m-p/1708585#M26286</guid>
      <dc:creator>hajianik</dc:creator>
      <dc:date>2023-08-21T21:20:29Z</dc:date>
    </item>
    <item>
      <title>Re: S32K310  PNE debugger</title>
      <link>https://community.nxp.com/t5/S32K/S32K310-PNE-debugger/m-p/1709726#M26380</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;this looks strange indeed. Be sure you are modifying right project in config tools; select right one from pull down list or double click on mex file from the project window. After changes click on Update Code.&amp;nbsp;&lt;BR /&gt;Compile project and check within Console if elf is generated finally. Then use debug configuration for this project and check if it points to elf generated.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Wed, 23 Aug 2023 08:46:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K310-PNE-debugger/m-p/1709726#M26380</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2023-08-23T08:46:19Z</dc:date>
    </item>
    <item>
      <title>Re: S32K310  PNE debugger</title>
      <link>https://community.nxp.com/t5/S32K/S32K310-PNE-debugger/m-p/1710148#M26405</link>
      <description>&lt;P&gt;Hi, I went through all the steps you mentioned, several times but no luck.&lt;/P&gt;&lt;P&gt;Anyways I HAD TO CREATE ANOTHER PROJECT based on the setting of&amp;nbsp; the bad project and so far it seems it is working properly.&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;</description>
      <pubDate>Wed, 23 Aug 2023 22:13:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K310-PNE-debugger/m-p/1710148#M26405</guid>
      <dc:creator>hajianik</dc:creator>
      <dc:date>2023-08-23T22:13:37Z</dc:date>
    </item>
  </channel>
</rss>