<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K312-Erase Flash Block Interface in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K312-Erase-Flash-Block-Interface/m-p/1708268#M26270</link>
    <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;When I use DS3.5 to generate C40 code to operate Flash, I found that there is only an interface for erasing Sector (C40_Ip_MainInterfaceSectorErase) in C40Ip.c, but I checked RM and found that bit[ESS] of register MCR can be set to erase Block of. Is there an interface to erase the Block?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BestRegards&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;</description>
    <pubDate>Mon, 21 Aug 2023 10:02:08 GMT</pubDate>
    <dc:creator>Simon-Liu</dc:creator>
    <dc:date>2023-08-21T10:02:08Z</dc:date>
    <item>
      <title>S32K312-Erase Flash Block Interface</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-Erase-Flash-Block-Interface/m-p/1708268#M26270</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;When I use DS3.5 to generate C40 code to operate Flash, I found that there is only an interface for erasing Sector (C40_Ip_MainInterfaceSectorErase) in C40Ip.c, but I checked RM and found that bit[ESS] of register MCR can be set to erase Block of. Is there an interface to erase the Block?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BestRegards&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;</description>
      <pubDate>Mon, 21 Aug 2023 10:02:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-Erase-Flash-Block-Interface/m-p/1708268#M26270</guid>
      <dc:creator>Simon-Liu</dc:creator>
      <dc:date>2023-08-21T10:02:08Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312-Erase Flash Block Interface</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-Erase-Flash-Block-Interface/m-p/1709005#M26310</link>
      <description>&lt;P&gt;In the RM 21.7.1.2, you may read statement that:&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;„Block erase is for Factory use only, under controlled conditions.“&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The Program/Erase cycles value is specified as 25, when using the Block Erase. That’s why flash drivers and external tools do not use this operation.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Aug 2023 09:58:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-Erase-Flash-Block-Interface/m-p/1709005#M26310</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2023-08-22T09:58:47Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312-Erase Flash Block Interface</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-Erase-Flash-Block-Interface/m-p/1709517#M26354</link>
      <description>&lt;P&gt;Thank you for your answer.&lt;/P&gt;&lt;P&gt;I saw this description in RM before, I thought that there was a way to enter the factory mode, now I understand that the block cannot be erased by the driver.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BestRegards&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;</description>
      <pubDate>Wed, 23 Aug 2023 03:21:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-Erase-Flash-Block-Interface/m-p/1709517#M26354</guid>
      <dc:creator>Simon-Liu</dc:creator>
      <dc:date>2023-08-23T03:21:23Z</dc:date>
    </item>
  </channel>
</rss>