<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックP-Flash and D-Flash</title>
    <link>https://community.nxp.com/t5/S32K/P-Flash-and-D-Flash/m-p/792093#M2624</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm using the s32k144evb and my application resides in P-Flash since it is to big to be stored directly in RAM ( It seems that if you use the SDK is very difficult to stay in the limits). Since I can't read simultaneously from P-Flash and D-Flash, should I put the D-Flash functions in RAM in order to be able to read it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If yes which is the method permiting me to put only some parts of code in ram?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NB:&lt;/P&gt;&lt;P&gt;The defined macro:&lt;/P&gt;&lt;P&gt;START_FUNCTION_DEFINITION_RAMSECTIOn&lt;/P&gt;&lt;P&gt;END_FUNCTION_DEFINITION_RAMSECTION&lt;/P&gt;&lt;P&gt;are defined as void with GCC compiler.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Jul 2018 11:44:36 GMT</pubDate>
    <dc:creator>alternativeunof</dc:creator>
    <dc:date>2018-07-27T11:44:36Z</dc:date>
    <item>
      <title>P-Flash and D-Flash</title>
      <link>https://community.nxp.com/t5/S32K/P-Flash-and-D-Flash/m-p/792093#M2624</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm using the s32k144evb and my application resides in P-Flash since it is to big to be stored directly in RAM ( It seems that if you use the SDK is very difficult to stay in the limits). Since I can't read simultaneously from P-Flash and D-Flash, should I put the D-Flash functions in RAM in order to be able to read it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If yes which is the method permiting me to put only some parts of code in ram?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NB:&lt;/P&gt;&lt;P&gt;The defined macro:&lt;/P&gt;&lt;P&gt;START_FUNCTION_DEFINITION_RAMSECTIOn&lt;/P&gt;&lt;P&gt;END_FUNCTION_DEFINITION_RAMSECTION&lt;/P&gt;&lt;P&gt;are defined as void with GCC compiler.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jul 2018 11:44:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/P-Flash-and-D-Flash/m-p/792093#M2624</guid>
      <dc:creator>alternativeunof</dc:creator>
      <dc:date>2018-07-27T11:44:36Z</dc:date>
    </item>
    <item>
      <title>Re: P-Flash and D-Flash</title>
      <link>https://community.nxp.com/t5/S32K/P-Flash-and-D-Flash/m-p/792094#M2625</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;What do you mean by the simultaneous reading of both D-Flash and P-Flash.&lt;BR /&gt;There is only one core and one Flash memory controller as a slave on the Crossbar switch (Figure 2-1 RM rev.8).&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/73153i1BB3E308260C3E4A/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So, you can execute code either from P-Flash or D-flash.&lt;BR /&gt;But it doesn’t mean that you can’t execute code form D-flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jul 2018 13:38:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/P-Flash-and-D-Flash/m-p/792094#M2625</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-07-30T13:38:08Z</dc:date>
    </item>
  </channel>
</rss>