<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K314 LpUart interrupt in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K314-LpUart-interrupt/m-p/1704700#M26065</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;You need to use the LPUART IDLE function. Maybe you can refer to the discussion in&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/The-S32K312-UART-DMA-IDLE-No-matter-which-UART-sends-data-is/td-p/1604940" target="_self"&gt;&lt;SPAN class="lia-link-navigation lia-link-disabled"&gt;The S32K312 UART+DMA+IDLE No matter which UART sends, data is sent as 0&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="lia-link-navigation lia-link-disabled"&gt;That project implement "UART receive indefinite length data".&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Tue, 15 Aug 2023 04:19:47 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2023-08-15T04:19:47Z</dc:date>
    <item>
      <title>S32K314 LpUart interrupt</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-LpUart-interrupt/m-p/1704283#M26040</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using S32K314 board, in our project we are connecting to a Modem in which we want to enable interrupt and read the bytes received in the UART. I am using Lpuart_Uart_Ip_AsyncReceive but I don't know the exact number of bytes that receiving through my AT commands. How to implement interrupt for a normal modem connection?&lt;/P&gt;</description>
      <pubDate>Mon, 14 Aug 2023 10:01:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-LpUart-interrupt/m-p/1704283#M26040</guid>
      <dc:creator>abhijith_r</dc:creator>
      <dc:date>2023-08-14T10:01:44Z</dc:date>
    </item>
    <item>
      <title>Re: S32K314 LpUart interrupt</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-LpUart-interrupt/m-p/1704700#M26065</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;You need to use the LPUART IDLE function. Maybe you can refer to the discussion in&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/The-S32K312-UART-DMA-IDLE-No-matter-which-UART-sends-data-is/td-p/1604940" target="_self"&gt;&lt;SPAN class="lia-link-navigation lia-link-disabled"&gt;The S32K312 UART+DMA+IDLE No matter which UART sends, data is sent as 0&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="lia-link-navigation lia-link-disabled"&gt;That project implement "UART receive indefinite length data".&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 15 Aug 2023 04:19:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-LpUart-interrupt/m-p/1704700#M26065</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-08-15T04:19:47Z</dc:date>
    </item>
  </channel>
</rss>