<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Question about BCTU CL in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Question-about-BCTU-CL/m-p/1704005#M26016</link>
    <description>&lt;P&gt;Hi Robin,&lt;/P&gt;&lt;P&gt;Thanks for your information. I am curious about the flexibility to execute a sequence conversion.&lt;/P&gt;&lt;P&gt;Using CL to sample a sequence of channels is used in BCTU conversion mode. The BCTU conversion mode has the highest priority's trigger and sends one trigger to start one conversion in CL.&lt;/P&gt;&lt;P&gt;If I use NCMR/JCMR, only one trigger is required for a sequence conversion. However the sequence must follow the ascending order of channels to sample.&lt;/P&gt;&lt;P&gt;Therefore, there is not a way to start a sequence of normal conversion in any order which only requires a trigger. That is my question.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;CK&lt;/P&gt;</description>
    <pubDate>Mon, 14 Aug 2023 03:59:48 GMT</pubDate>
    <dc:creator>CKing</dc:creator>
    <dc:date>2023-08-14T03:59:48Z</dc:date>
    <item>
      <title>Question about BCTU CL</title>
      <link>https://community.nxp.com/t5/S32K/Question-about-BCTU-CL/m-p/1702799#M25938</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;In S32K3xx, if I want to do a sequence of conversion on one ADC, I can use BCTU CL to configure a sequence and BCTU will&amp;nbsp;trigger ADC multiple times, or I can configure NCMRn/JCMRn to wait for a normal/injected trigger. Is the saying right?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;CK&lt;/P&gt;</description>
      <pubDate>Thu, 10 Aug 2023 08:48:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Question-about-BCTU-CL/m-p/1702799#M25938</guid>
      <dc:creator>CKing</dc:creator>
      <dc:date>2023-08-10T08:48:52Z</dc:date>
    </item>
    <item>
      <title>Re: Question about BCTU CL</title>
      <link>https://community.nxp.com/t5/S32K/Question-about-BCTU-CL/m-p/1703851#M26003</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;CK,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Sorry I may not understand your question.&lt;BR /&gt;Section&lt;STRONG&gt; 61.3.4.2 Operation modes in normal conversions&lt;/STRONG&gt; of &lt;A href="https://www.nxp.com/webapp/Download?colCode=S32K3XXRM" target="_self"&gt;S32K3XXRM&lt;/A&gt;(Rev.7) mentions that you can use One-Shot mode or Scan mode to implement &lt;U&gt;sequential conversion&lt;/U&gt;.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="61.3.4.2 Operation modes in normal conversions sequential conversion.png" style="width: 634px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/236163i8E11C24325D2019A/image-size/large?v=v2&amp;amp;px=999" role="button" title="61.3.4.2 Operation modes in normal conversions sequential conversion.png" alt="61.3.4.2 Operation modes in normal conversions sequential conversion.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;61.3.4.2 Operation modes in normal conversions sequential conversion.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Section &lt;STRONG&gt;65.3.2 Conversion list (CL)&lt;/STRONG&gt; of &lt;A href="https://www.nxp.com/webapp/Download?colCode=S32K3XXRM" target="_self"&gt;S32K3XXRM&lt;/A&gt; mentions:&lt;BR /&gt;A CL executes a &lt;U&gt;sequence of conversions&lt;/U&gt; on one or more target ADCs. It also stores information from the last conversion executed in a sequence except for the target ADC, which is stored in ADC select n (TRGCFG_m[ADC_SELn]).&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="65.3.2 Conversion list (CL) sequence of conversions.png" style="width: 702px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/236164iB0C4C70658094B31/image-size/large?v=v2&amp;amp;px=999" role="button" title="65.3.2 Conversion list (CL) sequence of conversions.png" alt="65.3.2 Conversion list (CL) sequence of conversions.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;65.3.2 Conversion list (CL) sequence of conversions.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;So I think either ADC normal conversions or BCTU CL can be used to sample a sequence of ADC channels.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Sun, 13 Aug 2023 02:01:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Question-about-BCTU-CL/m-p/1703851#M26003</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-08-13T02:01:44Z</dc:date>
    </item>
    <item>
      <title>Re: Question about BCTU CL</title>
      <link>https://community.nxp.com/t5/S32K/Question-about-BCTU-CL/m-p/1704005#M26016</link>
      <description>&lt;P&gt;Hi Robin,&lt;/P&gt;&lt;P&gt;Thanks for your information. I am curious about the flexibility to execute a sequence conversion.&lt;/P&gt;&lt;P&gt;Using CL to sample a sequence of channels is used in BCTU conversion mode. The BCTU conversion mode has the highest priority's trigger and sends one trigger to start one conversion in CL.&lt;/P&gt;&lt;P&gt;If I use NCMR/JCMR, only one trigger is required for a sequence conversion. However the sequence must follow the ascending order of channels to sample.&lt;/P&gt;&lt;P&gt;Therefore, there is not a way to start a sequence of normal conversion in any order which only requires a trigger. That is my question.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;CK&lt;/P&gt;</description>
      <pubDate>Mon, 14 Aug 2023 03:59:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Question-about-BCTU-CL/m-p/1704005#M26016</guid>
      <dc:creator>CKing</dc:creator>
      <dc:date>2023-08-14T03:59:48Z</dc:date>
    </item>
    <item>
      <title>Re: Question about BCTU CL</title>
      <link>https://community.nxp.com/t5/S32K/Question-about-BCTU-CL/m-p/1706138#M26148</link>
      <description>&lt;P&gt;61.3.4&amp;nbsp;Normal trigger&amp;nbsp;&lt;BR /&gt;Proceed through the standard input channels &lt;U&gt;in ascending order&lt;/U&gt;.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="61.3.4 Normal trigger in ascending order.png" style="width: 917px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/236756iA66CD51E3BFA50CA/image-size/large?v=v2&amp;amp;px=999" role="button" title="61.3.4 Normal trigger in ascending order.png" alt="61.3.4 Normal trigger in ascending order.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;61.3.4 Normal trigger in ascending order.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Unfortunately I didn't find which register to start a sequence of normal conversion &lt;U&gt;in any order&lt;/U&gt; which only requires a trigger.&lt;/P&gt;</description>
      <pubDate>Thu, 17 Aug 2023 02:04:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Question-about-BCTU-CL/m-p/1706138#M26148</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-08-17T02:04:29Z</dc:date>
    </item>
  </channel>
</rss>