<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32k14x UART flow control in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32k14x-UART-flow-control/m-p/1701018#M25858</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201913"&gt;@VaneB&lt;/a&gt;&amp;nbsp;I already checked that example. In same, standard SDK function are not used, direct registers are used in&amp;nbsp;setLpuartHardFlowCtrl().&lt;/P&gt;&lt;P&gt;Also can you answer this "&lt;SPAN&gt;&amp;nbsp;I understand that I have to configure these 2 pin for same with UART pin based on pinout MUX sheet. I want to understand does the control for these pin auto taken care by hardware based on usual&amp;nbsp;function&amp;nbsp;call like&amp;nbsp;LPUART_DRV_ReceiveData() and&amp;nbsp;LPUART_DRV_SendData()&amp;nbsp; or anything&amp;nbsp;extra needs to be done in application software"&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 08 Aug 2023 10:07:16 GMT</pubDate>
    <dc:creator>chandan_uv</dc:creator>
    <dc:date>2023-08-08T10:07:16Z</dc:date>
    <item>
      <title>S32k14x UART flow control</title>
      <link>https://community.nxp.com/t5/S32K/S32k14x-UART-flow-control/m-p/1700140#M25810</link>
      <description>&lt;P&gt;Hello, I am using S32K146 and want to implement UART with flow control (&lt;SPAN&gt;RTS and&amp;nbsp;CTS). I understand that I have to configure these 2 pin for same with UART pin based on pinout MUX sheet. I want to understand does the control for these pin auto taken care by hardware based on usual&amp;nbsp;function&amp;nbsp;call like&amp;nbsp;LPUART_DRV_ReceiveData() and&amp;nbsp;LPUART_DRV_SendData()&amp;nbsp; or anything&amp;nbsp;extra needs to be done in application software.&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 07 Aug 2023 10:03:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k14x-UART-flow-control/m-p/1700140#M25810</guid>
      <dc:creator>chandan_uv</dc:creator>
      <dc:date>2023-08-07T10:03:14Z</dc:date>
    </item>
    <item>
      <title>Re: S32k14x UART flow control</title>
      <link>https://community.nxp.com/t5/S32K/S32k14x-UART-flow-control/m-p/1700446#M25826</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/215611"&gt;@chandan_uv&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Unfortunately, the LPUART SDK driver does not support hardware flow control. But at&amp;nbsp;S32K Knowledge Base, you can find an example&amp;nbsp;to run on the S32K144EVB board with RTM 3.0.0.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/S32K-LPUART-hardware-flow-control/ta-p/1116812" target="_blank" rel="noopener"&gt;S32K LPUART hardware flow control&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Also, refer to sections 53.4.3.2 and&amp;nbsp;53.4.4.3 of the&amp;nbsp;S32K1xx Series Reference Manual.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R.&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;</description>
      <pubDate>Mon, 07 Aug 2023 20:49:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k14x-UART-flow-control/m-p/1700446#M25826</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-08-07T20:49:11Z</dc:date>
    </item>
    <item>
      <title>Re: S32k14x UART flow control</title>
      <link>https://community.nxp.com/t5/S32K/S32k14x-UART-flow-control/m-p/1701018#M25858</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201913"&gt;@VaneB&lt;/a&gt;&amp;nbsp;I already checked that example. In same, standard SDK function are not used, direct registers are used in&amp;nbsp;setLpuartHardFlowCtrl().&lt;/P&gt;&lt;P&gt;Also can you answer this "&lt;SPAN&gt;&amp;nbsp;I understand that I have to configure these 2 pin for same with UART pin based on pinout MUX sheet. I want to understand does the control for these pin auto taken care by hardware based on usual&amp;nbsp;function&amp;nbsp;call like&amp;nbsp;LPUART_DRV_ReceiveData() and&amp;nbsp;LPUART_DRV_SendData()&amp;nbsp; or anything&amp;nbsp;extra needs to be done in application software"&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 08 Aug 2023 10:07:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k14x-UART-flow-control/m-p/1701018#M25858</guid>
      <dc:creator>chandan_uv</dc:creator>
      <dc:date>2023-08-08T10:07:16Z</dc:date>
    </item>
    <item>
      <title>Re: S32k14x UART flow control</title>
      <link>https://community.nxp.com/t5/S32K/S32k14x-UART-flow-control/m-p/1702407#M25914</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/215611"&gt;@chandan_uv&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;As I mentioned before, the SDK does not support&amp;nbsp;hardware flow control.&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Aug 2023 21:13:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k14x-UART-flow-control/m-p/1702407#M25914</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-08-09T21:13:20Z</dc:date>
    </item>
    <item>
      <title>Re: S32k14x UART flow control</title>
      <link>https://community.nxp.com/t5/S32K/S32k14x-UART-flow-control/m-p/1773056#M29552</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201913"&gt;@VaneB&lt;/a&gt;&amp;nbsp;In that example,&amp;nbsp;&lt;SPAN&gt;CTS&amp;lt;-&amp;gt; RTS andCTS&amp;lt;-&amp;gt; RTS but generally they are ,&amp;nbsp;CTS&amp;lt;-&amp;gt; CTS and RTS&amp;lt;-&amp;gt; RTS connected. In that case, what should be changed in the code?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 12 Dec 2023 11:03:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k14x-UART-flow-control/m-p/1773056#M29552</guid>
      <dc:creator>chandan_uv</dc:creator>
      <dc:date>2023-12-12T11:03:37Z</dc:date>
    </item>
  </channel>
</rss>