<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックK396 EVB example error troubleshoot</title>
    <link>https://community.nxp.com/t5/S32K/K396-EVB-example-error-troubleshoot/m-p/1700723#M25841</link>
    <description>&lt;P&gt;Now i tested the demo example project of the S32 k396，and i found that after changing the pin and updating the generation code,then compliing it ,it shows the following error:&lt;/P&gt;&lt;P&gt;workspaceS32DS.3.5/Lighting_SingleCore_S32K396_M7/Lighting_SingleCore_S32K396_M7/swc/rte/generic/include/SwcRte.h:39:10: fatal error: SwcRte_Cfg.h: No such file or directory&lt;/P&gt;&lt;P&gt;SwcRte_Cfg.h file can be found out in the porject&amp;nbsp; before i updating the generation code,i want to know why it miss after i clicking the update button of the S32 v3.5?What should i do to solve this error?&lt;/P&gt;</description>
    <pubDate>Tue, 08 Aug 2023 05:58:17 GMT</pubDate>
    <dc:creator>Harry0001</dc:creator>
    <dc:date>2023-08-08T05:58:17Z</dc:date>
    <item>
      <title>K396 EVB example error troubleshoot</title>
      <link>https://community.nxp.com/t5/S32K/K396-EVB-example-error-troubleshoot/m-p/1700723#M25841</link>
      <description>&lt;P&gt;Now i tested the demo example project of the S32 k396，and i found that after changing the pin and updating the generation code,then compliing it ,it shows the following error:&lt;/P&gt;&lt;P&gt;workspaceS32DS.3.5/Lighting_SingleCore_S32K396_M7/Lighting_SingleCore_S32K396_M7/swc/rte/generic/include/SwcRte.h:39:10: fatal error: SwcRte_Cfg.h: No such file or directory&lt;/P&gt;&lt;P&gt;SwcRte_Cfg.h file can be found out in the porject&amp;nbsp; before i updating the generation code,i want to know why it miss after i clicking the update button of the S32 v3.5?What should i do to solve this error?&lt;/P&gt;</description>
      <pubDate>Tue, 08 Aug 2023 05:58:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/K396-EVB-example-error-troubleshoot/m-p/1700723#M25841</guid>
      <dc:creator>Harry0001</dc:creator>
      <dc:date>2023-08-08T05:58:17Z</dc:date>
    </item>
    <item>
      <title>Re: K396 EVB example error troubleshoot</title>
      <link>https://community.nxp.com/t5/S32K/K396-EVB-example-error-troubleshoot/m-p/1700783#M25846</link>
      <description>&lt;P&gt;it seems that before it is called "&lt;SPAN&gt;SwcRte_Cfg&lt;/SPAN&gt;",after updating it change to "SwcRte_PBcfg"!Should i rename it name to "SwcRte_cfg"?&lt;/P&gt;</description>
      <pubDate>Tue, 08 Aug 2023 06:50:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/K396-EVB-example-error-troubleshoot/m-p/1700783#M25846</guid>
      <dc:creator>Harry0001</dc:creator>
      <dc:date>2023-08-08T06:50:01Z</dc:date>
    </item>
    <item>
      <title>Re: K396 EVB example error troubleshoot</title>
      <link>https://community.nxp.com/t5/S32K/K396-EVB-example-error-troubleshoot/m-p/1701595#M25885</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;That is because your project is generated as post build (PBcfg) instead of precompile (CFG).&lt;/P&gt;
&lt;P&gt;Those are 2 basic AUTOSAR structures for project generation.&lt;/P&gt;
&lt;P&gt;Please select the precompile one in order to get CFG files linked.&lt;/P&gt;
&lt;P&gt;For more details please refer to basic autosar trainings.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Wed, 09 Aug 2023 06:27:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/K396-EVB-example-error-troubleshoot/m-p/1701595#M25885</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2023-08-09T06:27:01Z</dc:date>
    </item>
    <item>
      <title>Re: K396 EVB example error troubleshoot</title>
      <link>https://community.nxp.com/t5/S32K/K396-EVB-example-error-troubleshoot/m-p/1702921#M25949</link>
      <description>&lt;P&gt;&lt;SPAN&gt;“Please select the precompile one in order to get CFG files linked.&lt;/SPAN&gt;”&lt;/P&gt;&lt;P&gt;Please tell me where to chose the precompile setting,i am confused for that.&lt;/P&gt;&lt;P&gt;Other question is that i cannot find the file for S32 opening but only finding the example file for EB,as is the attached picture showing,i have downloaded the updated software package which updated time is April,2023 ,what is the point of this problem?Thanks!&lt;/P&gt;</description>
      <pubDate>Thu, 10 Aug 2023 11:29:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/K396-EVB-example-error-troubleshoot/m-p/1702921#M25949</guid>
      <dc:creator>Harry0001</dc:creator>
      <dc:date>2023-08-10T11:29:35Z</dc:date>
    </item>
    <item>
      <title>Re: K396 EVB example error troubleshoot</title>
      <link>https://community.nxp.com/t5/S32K/K396-EVB-example-error-troubleshoot/m-p/1703345#M25959</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;Please tell me where to chose the precompile setting,i am confused for that&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;You can select it in your configuration tool. For example:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="petervlna_0-1691736545645.png" style="width: 498px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/236053i162E9F874ED17B1E/image-dimensions/498x329?v=v2" width="498" height="329" role="button" title="petervlna_0-1691736545645.png" alt="petervlna_0-1691736545645.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;petervlna_0-1691736545645.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;Other question is that i cannot find the file for S32 opening but only finding the example file for EB&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Well hard to say. I could be that there are no S32DS examples. But the sample SW is usually provided directly in plugins:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="petervlna_1-1691737166952.png" style="width: 506px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/236054i1FE19A4AA85D2701/image-dimensions/506x210?v=v2" width="506" height="210" role="button" title="petervlna_1-1691737166952.png" alt="petervlna_1-1691737166952.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;petervlna_1-1691737166952.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Aug 2023 06:59:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/K396-EVB-example-error-troubleshoot/m-p/1703345#M25959</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2023-08-11T06:59:44Z</dc:date>
    </item>
  </channel>
</rss>