<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K324 Crypto returns CRYPTO_RET_OPERATION_TIMEOUT in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K324-Crypto-returns-CRYPTO-RET-OPERATION-TIMEOUT/m-p/1700655#M25834</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I refer to the demo of Crypto_SymmetricPrimitives_S32K44 to use S32K324's Crypto module, but it can't run it correctly. I trace the code to find that it is timeout in the function of Hse_Ip_ServiceRequest.&lt;/P&gt;&lt;P&gt;/* Send the request to HSE driver */&lt;BR /&gt;HseResponse = Hse_Ip_ServiceRequest(u8MuInstance, u8MuChannel, pHseIpReq, pHseSrvDescriptor);&lt;BR /&gt;/* Translate the message received from HSE to a Std_ReturnType value */&lt;BR /&gt;RetVal = Crypto_Hse_TranslateHseResponse(HseResponse);&lt;/P&gt;&lt;P&gt;RetVal is the value of&amp;nbsp;CRYPTO_RET_OPERATION_TIMEOUT. So I don't kown what the probelm is.&lt;/P&gt;&lt;P&gt;Are there any configurations that affect this function?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 08 Aug 2023 03:14:35 GMT</pubDate>
    <dc:creator>Faker</dc:creator>
    <dc:date>2023-08-08T03:14:35Z</dc:date>
    <item>
      <title>S32K324 Crypto returns CRYPTO_RET_OPERATION_TIMEOUT</title>
      <link>https://community.nxp.com/t5/S32K/S32K324-Crypto-returns-CRYPTO-RET-OPERATION-TIMEOUT/m-p/1700655#M25834</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I refer to the demo of Crypto_SymmetricPrimitives_S32K44 to use S32K324's Crypto module, but it can't run it correctly. I trace the code to find that it is timeout in the function of Hse_Ip_ServiceRequest.&lt;/P&gt;&lt;P&gt;/* Send the request to HSE driver */&lt;BR /&gt;HseResponse = Hse_Ip_ServiceRequest(u8MuInstance, u8MuChannel, pHseIpReq, pHseSrvDescriptor);&lt;BR /&gt;/* Translate the message received from HSE to a Std_ReturnType value */&lt;BR /&gt;RetVal = Crypto_Hse_TranslateHseResponse(HseResponse);&lt;/P&gt;&lt;P&gt;RetVal is the value of&amp;nbsp;CRYPTO_RET_OPERATION_TIMEOUT. So I don't kown what the probelm is.&lt;/P&gt;&lt;P&gt;Are there any configurations that affect this function?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 08 Aug 2023 03:14:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K324-Crypto-returns-CRYPTO-RET-OPERATION-TIMEOUT/m-p/1700655#M25834</guid>
      <dc:creator>Faker</dc:creator>
      <dc:date>2023-08-08T03:14:35Z</dc:date>
    </item>
    <item>
      <title>Re: S32K324 Crypto returns CRYPTO_RET_OPERATION_TIMEOUT</title>
      <link>https://community.nxp.com/t5/S32K/S32K324-Crypto-returns-CRYPTO-RET-OPERATION-TIMEOUT/m-p/1701255#M25865</link>
      <description>&lt;P&gt;H i&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/179808"&gt;@Faker&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;To be able to run the example, you need to have installed the HSE FW.&lt;/P&gt;
&lt;P&gt;As you are having a timeout at&amp;nbsp;&lt;SPAN&gt;Hse_Ip_ServiceRequest, which means that is expecting the response of the HSE and is not getting it.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Please make sure to have installed the HSE FW before running the example code.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;B.R.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;VaneB.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 08 Aug 2023 17:19:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K324-Crypto-returns-CRYPTO-RET-OPERATION-TIMEOUT/m-p/1701255#M25865</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2023-08-08T17:19:02Z</dc:date>
    </item>
  </channel>
</rss>