<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K144 LPSPI Transfer in 16bit mode in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-LPSPI-Transfer-in-16bit-mode/m-p/789301#M2581</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello ,&lt;/P&gt;&lt;P&gt;I configured LPSPI Driver to transmit some dummy 16bit data on MOSI and its working(measured on CRO).&lt;/P&gt;&lt;P&gt;I have one doubt with respect to MISO capture?Is LPSPI will support Full duplex communication means in one instance i can put the data on MOSI and as well as i can read data on MISO?&lt;/P&gt;&lt;P&gt;or in First instance(16 clocks) i need to send data and in next instance(16clocks), i must read data on MISO?&lt;/P&gt;&lt;P&gt;Actually, I want to establish LPSPI 16bit communication with SBC(FS45xx).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Dec 2018 08:20:24 GMT</pubDate>
    <dc:creator>phanendravarma_</dc:creator>
    <dc:date>2018-12-12T08:20:24Z</dc:date>
    <item>
      <title>S32K144 LPSPI Transfer in 16bit mode</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-LPSPI-Transfer-in-16bit-mode/m-p/789301#M2581</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello ,&lt;/P&gt;&lt;P&gt;I configured LPSPI Driver to transmit some dummy 16bit data on MOSI and its working(measured on CRO).&lt;/P&gt;&lt;P&gt;I have one doubt with respect to MISO capture?Is LPSPI will support Full duplex communication means in one instance i can put the data on MOSI and as well as i can read data on MISO?&lt;/P&gt;&lt;P&gt;or in First instance(16 clocks) i need to send data and in next instance(16clocks), i must read data on MISO?&lt;/P&gt;&lt;P&gt;Actually, I want to establish LPSPI 16bit communication with SBC(FS45xx).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Dec 2018 08:20:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-LPSPI-Transfer-in-16bit-mode/m-p/789301#M2581</guid>
      <dc:creator>phanendravarma_</dc:creator>
      <dc:date>2018-12-12T08:20:24Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 LPSPI Transfer in 16bit mode</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-LPSPI-Transfer-in-16bit-mode/m-p/789302#M2582</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Yes, the LPSPI support full-duplex mode, simultaneous transfers in both directions.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Dec 2018 09:35:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-LPSPI-Transfer-in-16bit-mode/m-p/789302#M2582</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-12-12T09:35:23Z</dc:date>
    </item>
  </channel>
</rss>