<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K144 Q100 openSDA application issue.</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-Q100-openSDA-application-issue/m-p/1698963#M25762</link>
    <description>&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;I'm trying to download a bin file from a vendor to my S32K144 development board.&lt;BR /&gt;So, after making a USB connection between S32K144 &amp;lt;-&amp;gt; PC, I copied that BIN file to the S32K144 folder.&lt;/P&gt;&lt;P&gt;However, the OPENSDA LED blinked 8 times and then turned off for 2 seconds.&lt;BR /&gt;According to the OPENSDAUG file, this is an error phenomenon.&lt;/P&gt;&lt;P&gt;How can I install the bin file normally without this problem?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Fri, 04 Aug 2023 01:15:11 GMT</pubDate>
    <dc:creator>sjshin</dc:creator>
    <dc:date>2023-08-04T01:15:11Z</dc:date>
    <item>
      <title>S32K144 Q100 openSDA application issue.</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-Q100-openSDA-application-issue/m-p/1698963#M25762</link>
      <description>&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;I'm trying to download a bin file from a vendor to my S32K144 development board.&lt;BR /&gt;So, after making a USB connection between S32K144 &amp;lt;-&amp;gt; PC, I copied that BIN file to the S32K144 folder.&lt;/P&gt;&lt;P&gt;However, the OPENSDA LED blinked 8 times and then turned off for 2 seconds.&lt;BR /&gt;According to the OPENSDAUG file, this is an error phenomenon.&lt;/P&gt;&lt;P&gt;How can I install the bin file normally without this problem?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Fri, 04 Aug 2023 01:15:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-Q100-openSDA-application-issue/m-p/1698963#M25762</guid>
      <dc:creator>sjshin</dc:creator>
      <dc:date>2023-08-04T01:15:11Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 Q100 openSDA application issue.</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-Q100-openSDA-application-issue/m-p/1699074#M25769</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Please refer to the discussion in&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/S32K144-D2-RED-LED-is-ON-always/m-p/1567621" target="_self"&gt;S32K144 D2 RED LED is ON always&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If your computer is Win10, please Disable/stop Windows Services by refer to&amp;nbsp;&lt;A href="https://mcuoneclipse.com/2018/04/10/recovering-opensda-boards-with-windows-10/" target="_self"&gt;Recovering OpenSDA Boards with Windows 10&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 04 Aug 2023 04:30:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-Q100-openSDA-application-issue/m-p/1699074#M25769</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-08-04T04:30:22Z</dc:date>
    </item>
  </channel>
</rss>